2010-01-18 10:23 AM
Clock problem of SysTick Timer for 1 sn
2011-05-17 4:03 AM
There is an example on the address ''C:\Keil\ARM\Examples\ST\STM32F10x\NVIC\Example3'' .This application uses SysTick Timer to make an interrupt every 1 sn.There is no clock source adjustment for SysTick timer,so default clock source is used(HCLK/8 --> 72 Mz / 8= 9 Mhz)Set up code lines for SysTick timer is shown on the below.
/* SysTick interrupt each 1 Hz with Counter clock equal to 72MHz/8 = 9MHz */ SysTick_SetReload(9000000); I tried this application on MCBSTM32 kit.I made toggle a led connected to PortB (PB8) instead of PortC.But the delay between led's toggle positions was more than 1 sn.(nearly 8 sn )I added the code ''SysTick_CLKSourceConfig(SysTick_CLKSource_HCLK);.Delay become just 1 sn this time.But it's value should have be 1/10 sn . What is the wrong with this application? Best Regards;2011-05-17 4:03 AM
I am also having this problem. My clock tree is as follows:
OSC_IN(8MHz) | (x9)PLLMUL | SYSCLK | (/1)AHB Prescaler Therefore my Cortex System Timer will be running at 9MHz. When the SysTick registers are setup in the following manner, I do not get a 1ms interrupt. __INLINE static void init_SysTick(void) { SysTick->LOAD = 0x0089543F; //8999999dec SysTick->CTRL = 0x00000007; } The interrupt is firing, but its much slower than 1ms. Have I overlooked something?We’re moving the ST Community to a new platform to give you a better and more reliable community experience.