2015-02-22 8:49 AM
Hi, I'm currently trying to send data from one STM32F4 board as a master to the other STM32F4 board which is the slave via SPI.
However recever data are incorect.
//************************Code Master************************************void spi_init() { GPIO_InitTypeDef gpio; SPI_InitTypeDef spi1; RCC_AHB1PeriphClockCmd(RCC_AHB1Periph_GPIOA,ENABLE); RCC_APB2PeriphClockCmd(RCC_APB2Periph_SPI1,ENABLE); GPIO_StructInit(&gpio); gpio.GPIO_Pin = GPIO_Pin_5 | GPIO_Pin_6 | GPIO_Pin_7; gpio.GPIO_Mode = GPIO_Mode_AF; gpio.GPIO_Speed = GPIO_Speed_50MHz; gpio.GPIO_OType = GPIO_OType_PP; gpio.GPIO_PuPd = GPIO_PuPd_DOWN; GPIO_Init(GPIOA,&gpio); GPIO_PinAFConfig(GPIOA,GPIO_PinSource5,GPIO_AF_SPI1); GPIO_PinAFConfig(GPIOA,GPIO_PinSource6,GPIO_AF_SPI1); GPIO_PinAFConfig(GPIOA,GPIO_PinSource7,GPIO_AF_SPI1); SPI_I2S_DeInit(SPI1); SPI_StructInit(&spi1); spi1.SPI_Mode = SPI_Mode_Master; spi1.SPI_DataSize = SPI_DataSize_16b; spi1.SPI_NSS = SPI_NSS_Soft; SPI_Init(SPI1,&spi1); SPI_Cmd(SPI1,ENABLE);}void spi_send(uint16_t data) { SPI_I2S_SendData(SPI1,data); while(SPI_I2S_GetFlagStatus(SPI1,SPI_I2S_FLAG_TXE) == RESET); }int main() {spi_init(); STM_EVAL_LEDInit(LED3); STM_EVAL_LEDOn(LED3); while(1)
{ spi_send(0x0001); } return 0;}
//******************************Code Slave****************************************
uint16_t data = 0x0000;void spi_init() { GPIO_InitTypeDef gpio; SPI_InitTypeDef spi2; RCC_AHB1PeriphClockCmd(RCC_AHB1Periph_GPIOB,ENABLE); RCC_APB1PeriphClockCmd(RCC_APB1Periph_SPI2,ENABLE); GPIO_StructInit(&gpio); gpio.GPIO_Pin = GPIO_Pin_13 | GPIO_Pin_14 | GPIO_Pin_15; gpio.GPIO_Mode = GPIO_Mode_AF; gpio.GPIO_Speed = GPIO_Speed_50MHz; gpio.GPIO_OType = GPIO_OType_PP; gpio.GPIO_PuPd = GPIO_PuPd_DOWN; GPIO_Init(GPIOB,&gpio); GPIO_PinAFConfig(GPIOB,GPIO_PinSource13,GPIO_AF_SPI2); GPIO_PinAFConfig(GPIOB,GPIO_PinSource14,GPIO_AF_SPI2); GPIO_PinAFConfig(GPIOB,GPIO_PinSource15,GPIO_AF_SPI2); SPI_I2S_DeInit(SPI2); SPI_StructInit(&spi2); spi2.SPI_Mode = SPI_Mode_Slave; spi2.SPI_DataSize = SPI_DataSize_16b; spi2.SPI_NSS = SPI_NSS_Soft; SPI_Init(SPI2,&spi2); SPI_Cmd(SPI2,ENABLE);} uint16_t spi_receve() { uint16_t received ; while (SPI_I2S_GetFlagStatus(SPI2, SPI_I2S_FLAG_RXNE) == RESET); received = SPI_I2S_ReceiveData(SPI2); return received;}int main() { spi_init(); STM_EVAL_LEDInit(LED3); while(1) { data = spi_receve(); //data are correct
0x0800....0x0008....0x0000 if (data == 0x0001) STM_EVAL_LEDOn(LED3); } return 0;}///////////////////////////////Help me please.....thanks #stm32f4-discoveryWe’re moving the ST Community to a new platform to give you a better and more reliable community experience.