2024-01-05 7:49 AM
Hello,
I am trying to generate spi clock(100kz) in stm32g473,but desired output not getting in DSO .I tried to change stm32cubemx configuration then i changed the user code then also not getting desired output.
Please help me what changes I needed to generate clock.
Thank you in advance.
2024-01-05 8:01 AM
It's impossible to suggest the changes without seeing the code. SPI clock is output only when you send the data. SPI will not output the clock signal unless you transmit something.
2024-01-05 8:03 AM - edited 2024-01-05 8:04 AM
Read out and check/post content of SPI and relevant GPIO registers.
What hardware? You can check proper connection of SPI_SCK by setting given pin to GPIO Output and toggling "manually" (i.e. doing a basic "blinky").
JW
2024-01-05 9:25 PM - edited 2024-01-05 9:48 PM
here is configuration i did in the stm32cubemx
void MX_SPI1_Init(void)
{
hspi1.Instance = SPI1;
hspi1.Init.Mode = SPI_MODE_MASTER;
hspi1.Init.Direction = SPI_DIRECTION_2LINES;
hspi1.Init.DataSize = SPI_DATASIZE_8BIT;
hspi1.Init.CLKPolarity = SPI_POLARITY_LOW;
hspi1.Init.CLKPhase = SPI_PHASE_1EDGE;
hspi1.Init.NSS = SPI_NSS_SOFT;
hspi1.Init.BaudRatePrescaler = SPI_BAUDRATEPRESCALER_128;
hspi1.Init.FirstBit = SPI_FIRSTBIT_MSB;
hspi1.Init.TIMode = SPI_TIMODE_DISABLE;
hspi1.Init.CRCCalculation = SPI_CRCCALCULATION_DISABLE;
hspi1.Init.CRCPolynomial = 7;
hspi1.Init.CRCLength = SPI_CRC_LENGTH_DATASIZE;
hspi1.Init.NSSPMode = SPI_NSS_PULSE_DISABLE;
if (HAL_SPI_Init(&hspi1) != HAL_OK)
{
Error_Handler();
}
}
void HAL_SPI_MspInit(SPI_HandleTypeDef* spiHandle)
{
GPIO_InitTypeDef GPIO_InitStruct = {0};
if(spiHandle->Instance==SPI1)
{
/* USER CODE BEGIN SPI1_MspInit 0 */
/* USER CODE END SPI1_MspInit 0 */
/* SPI1 clock enable */
__HAL_RCC_SPI1_CLK_ENABLE();
__HAL_RCC_GPIOA_CLK_ENABLE();
/**SPI1 GPIO Configuration
PA5 ------> SPI1_SCK
PA6 ------> SPI1_MISO
PA7 ------> SPI1_MOSI
*/
GPIO_InitStruct.Pin = GPIO_PIN_5|GPIO_PIN_6|GPIO_PIN_7;
GPIO_InitStruct.Mode = GPIO_MODE_AF_PP;
GPIO_InitStruct.Pull = GPIO_PULLUP;
GPIO_InitStruct.Speed = GPIO_SPEED_FREQ_LOW;
GPIO_InitStruct.Alternate = GPIO_AF5_SPI1;
HAL_GPIO_Init(GPIOA, &GPIO_InitStruct);
/* USER CODE BEGIN SPI1_MspInit 1 */
/* USER CODE END SPI1_MspInit 1 */
}
}
void MX_GPIO_Init(void)
{
GPIO_InitTypeDef GPIO_InitStruct = {0};
/* GPIO Ports Clock Enable */
__HAL_RCC_GPIOF_CLK_ENABLE();
__HAL_RCC_GPIOA_CLK_ENABLE();
/*Configure GPIO pin Output Level */
HAL_GPIO_WritePin(GPIOA, GPIO_PIN_4, GPIO_PIN_RESET);
/*Configure GPIO pin : PA4 */
GPIO_InitStruct.Pin = GPIO_PIN_4;
GPIO_InitStruct.Mode = GPIO_MODE_OUTPUT_PP;
GPIO_InitStruct.Pull = GPIO_PULLUP;
GPIO_InitStruct.Speed = GPIO_SPEED_FREQ_LOW;
HAL_GPIO_Init(GPIOA, &GPIO_InitStruct);
}
user code
while (1)
{
/* USER CODE END WHILE */
/* USER CODE BEGIN 3 */
HAL_GPIO_WritePin(GPIOA,GPIO_PIN_4,GPIO_PIN_SET);
HAL_GPIO_WritePin(GPIOA,GPIO_PIN_4,GPIO_PIN_RESET);
HAL_Delay(1000);
HAL_SPI_Transmit(&hspi1,&data,1,HAL_MAX_DELAY);
HAL_GPIO_WritePin(GPIOA,GPIO_PIN_4,GPIO_PIN_SET);
HAL_Delay(1000);
}
/* USER CODE END 3 */
}
2024-01-06 1:03 AM
yes i tried this clock is toggling.
2024-01-06 1:40 AM - edited 2024-01-06 1:41 AM
Hi,
Just to clarify: you send 1 byte every 2 seconds ;
set data to something ? like : 0xAA , then you see some pulses on data line ?
+ 8 pulses on clk line ? ( every 2 seconds )
2024-01-07 12:39 AM
I declared data variable to 0xAA in above code
But no any pulses on data line .
2024-01-07 12:55 AM
Read out and check/post content of SPI and relevant GPIO registers.
JW
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.