2011-11-22 5:23 PM
Is there a simple example of this?
I've written some code based on a working non-DMA version of my SPI object. So far I have the following:void SPI2_StartDMA(u16 NumBytes){ // Disable both DMA channels DMA1_Stream3->CR &= ~1; DMA1_Stream4->CR &= ~1; // Disable the SPI port SPI2->CR1 &= ~0x40; // Clear any outstanding DMA interrupts DMA1->LIFCR = 0x0F400000; DMA1->HIFCR = 0x0000003D; // Configure the receiver DMA1_Stream3->CR = (DMA1_Stream3->CR & 0xF0100000) | 0x00012C20; DMA1_Stream3->NDTR = NumBytes; DMA1_Stream3->PAR = (uint32_t)&(SPI2->DR); DMA1_Stream3->M0AR = (uint32_t)&(SPI2RxBuf[0]); // Configure the transmitter DMA1_Stream4->CR = (DMA1_Stream4->CR & 0xF0100000) | 0x00012C60; DMA1_Stream4->NDTR = NumBytes; DMA1_Stream4->PAR = (uint32_t)&(SPI2->DR); DMA1_Stream4->M0AR = (uint32_t)&(SPI2TxBuf[0]); // Flush the SPI receiver (void)SPI2->DR; // Enable the DMA mode in the SPI SPI2->CR2 |= 3; // Enable the DMA devices DMA1_Stream3->CR |= 1; DMA1_Stream4->CR |= 1; // Enable the SPI Port - to start the transfer SPI2->CR1 |= 0x40; }I call the previous function with something like: SPI2TxBuf[0] = 10; SPI2TxBuf[1] = 0; SPI2TxBuf[2] = 55;SPI2_StartDMA(3); // Tx/Rx 3 bytes // Wait for the received response
printf(''Wait.'');
while ((DMA1->LISR & 0x0B400000) == 0) ;printf(''Success.'');
I get ''Wait.'', but no ''Success.''. It's like the process hasn't started.
Any ideas as to what I might be doing wrong?2011-11-22 11:13 PM
Hi
Did you setup your SPI to support DMA for transmitting and receiving? Is the receiver FIFO setup correct? Regards Raphael2011-11-22 11:41 PM
Hi Raphael,
In answer to your questions, the code I attached includes:// Enable the DMA mode in the SPI
SPI2->CR2 |= 3;
andDMA1_Stream3->M0AR = (uint32_t)&(SPI2RxBuf[0]);
...
DMA1_Stream4->M0AR = (uint32_t)&(SPI2TxBuf[0]);
Which I believe answers both your questions.SPI2RxBuf[0] and
SPI2TxBuf[0] are defined as simple arrays.
I know the SPI port works, because my port-bashed non-DMA version of the driver works fine.2011-11-23 3:08 AM
Solved.
In the end it was a simple misunderstanding of the role of peripheral control versus DMA control of the flow controller. The solution was to change the following lines:DMA1_Stream3->CR = (DMA1_Stream3->CR & 0xF0100000) | 0x00012C00;
...DMA1_Stream4->CR = (DMA1_Stream4->CR & 0xF0100000) | 0x00012C40;
Blink and you'll miss the change. But making this change resulted in the DMA jumping into life!This processor is so cool - even if a bit mind-numbing at times.We’re moving the ST Community to a new platform to give you a better and more reliable community experience.