2016-09-11 7:31 PM
The problem is that I have an *external* 24.576 MHz MCLK. In master mode, how do I get that from outside the chip onto the SAI_CK_A or SAI_CK_B clock?
I was going through section 36.3.1 ''SAI block diagram'' and figuring out how to wire everything up.If the STM32F7 is a slave, things mostly make sense: SCK maps to BCLK, FS maps to FCLK or LRCLK, SD maps to data. Presumably, MCLK is ignored--that's a little scary but I guess it could work given that the audio block has FIFOs.If the STM32F7 is a master *AND* generates the clock, then things are perfectly straightforward: MCLK is generated and maps to MCLK, SCK maps to BCLK, FS maps to FCLK or LRCLK, SD maps to data. The reference manual mumbles in section 36.3.7:The clock source for the clock generator comes from the product clock controller.
Okaaaay. I don't see anything in the manual about an SAI product clock controller. Nothing is listed which directly drives SAI_CK_x in Figure 429.Any help would be appreciated.Thanks. #sai-mclk-m7-stm32f72016-09-12 3:05 AM
> The problem is that I have an *external* 24.576 MHz MCLK. In master mode, how do I get that from outside the chip onto the SAI_CK_A or SAI_CK_B clock?
You don't need to. The high-frequency ''master'' clocks in codecs drive the oversampled sampler and filters; they are not needed to transfer data. > The reference manual mumbles in section 36.3.7:> The clock source for the clock generator comes from the product clock controller.
It's a bad way to say ''clock comes from RCC''. JW PS. When referring to RM, post number of RM and revision - note that there are several different RMs for various groups of STM32F7.2016-09-12 1:38 PM
Oh, thanks for the reference.
But, crud, the only pin to run an external MCLK seems to be I2S_CKIN and that is attached to exactly one and only one pin on the TQFP144. And that's being used by my sdcard interface (Figure 12-page 150). Erm. Guess I'm going to be trying to run the STM32F7 in slave mode then.Thanks for the pointers though.Relevant Reference manual ID:DocID028270 Rev 2
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.