2015-06-27 2:49 AM
I want to know
if code
made
the
discovery
STM32F303VCT6
(
) nottaking advantage of the
function
of the
discovery
kit
,in
which model
of
core
compiles
without
making any changes
.Where it compile ? Only
on the
NUCLEO
-
F303REor
even on the
NUCLEO
-
F411RE
.
Thanks !! #nucleo #stm32f3discovery2015-06-30 3:26 AM
Hi,
you can take the firmware of discovery STM32F303VCT6 to use it for NUCLEO-
F303RE, but it is not possible to use a firmware dedicated to F3 series with F4 series. However, you can download the Cube package for discovery and nucleo based on F3 and the cube package for discovery and nucleo based on F4. Hope the response has clarified the issue. Regards2015-07-03 4:11 AM
Hi,
now it is clearer to me. Software developed for STM32F411RE can run on STM32F407VGT6, using STM32CubeF4. The same applies to NUCLEO-F303RE and STM32F303VCT6, using STM32CubeF3. Some things are not clear to me yet: 1. Before the developing of Cube, with which firmware were Nucleo boards programmed? 2. The Getting Started with STM32? Nucleo Boatd Software Development Tools guide refers to STM32 Nucleo_FW_VX.Y.Z, that I did non find. Is it perhaps not available anymore? 3. To program my F3 or F4, I do not want to use the related Cube softare, rather the Discovery firmware, or the low level libraries for F3 and F4 (CMSIS). For example, I wrote a simple program that turns on and off an intagrated led of STM32F407VGT6, using the Discovery Kit Firmware, will it work, appropriately changing related GPIO and Pin, on STM32F411RE? I attach it for clarity. /#include ''stm32f4_discovery.h'' #include ''main.h'' GPIO_InitTypeDef GPIO_InitStructure; void Delay(__IO uint32_t nCount); int main(void) { /* GPIOD Periph clock enable in STM32F407VGT6 */ /* GPIOA Periph clock enable in STM32F411RE */ RCC_AHB1PeriphClockCmd(RCC_AHB1Periph_GPIOA, ENABLE); /* Configure PD12 in output pushpull mode in STM32F407VGT6 */ /* Configure PA5 in output pushpull mode in STM32F411RE */ GPIO_InitStructure.GPIO_Pin = GPIO_Pin_5; GPIO_InitStructure.GPIO_Mode = GPIO_Mode_OUT; GPIO_InitStructure.GPIO_OType = GPIO_OType_PP; GPIO_InitStructure.GPIO_Speed = GPIO_Speed_100MHz; GPIO_InitStructure.GPIO_PuPd = GPIO_PuPd_NOPULL; GPIO_Init(GPIOA, &GPIO_InitStructure); while (1) { /* PD12 to be toggled in STM32F407VGT6 */ // GPIO_TogglePin(GPIOD, GPIO_PIN_12); /* PA5 to be toggled in in STM32F411RE */ GPIO_TogglePin(GPIOA, GPIO_PIN_5); /* Insert delay */ Delay(0x3FFFFF); } } void Delay(__IO uint32_t nCount) { while(nCount--) { } } #ifdef USE_FULL_ASSERT void assert_failed(uint8_t* file, uint32_t line) { while (1) { } } #endif Thank you for clarifying my issues.2015-07-06 7:29 AM
Hi,
1-To my knowledge, some Nucleo boards were developed with Standard peripheral Library. New ones are developed only with cube package. 2-Under the UM1726 , in the introcuction they mention ''STSW-STM32143'', this firmware can be dowloaded from , when you unzip it you willfinf the STM32 Nucleo_FW_VX.Y.Z folder. 3-If I undersantand, you can develop your own application for F4/F3 with only using the CMSIS library. RegardsWe’re moving the ST Community to a new platform to give you a better and more reliable community experience.