2022-01-19 8:06 AM
Hi there,
I'm trying to implement a software interrupt using the STM32L432KC. I want to trigger an interrupt when I reach a certain point in the code. Unfortunately I didn't find any helpful example.
Once I tried to set bit37 in the IMR2 register.
SET_BIT(EXTI->IMR2 , EXTI_IMR2_IM37_Msk);
and am assumed that when setting the same bit by name in the SWIER register triggers the interrupt.
SET_BIT(EXTI->SWIER2 , EXTI_SWIER2_SWI37_Msk);
But it doesn't work. The program does not jump into the function
void SVC_Handler (void)
Can someone explain to me how to do this!?
Solved! Go to Solution.
2022-01-19 8:13 AM
Software Trigger Interrupt Register (STIR)
https://stackoverflow.com/questions/44482964/using-exti-line-for-software-interrupt
2022-01-19 8:13 AM
Software Trigger Interrupt Register (STIR)
https://stackoverflow.com/questions/44482964/using-exti-line-for-software-interrupt
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.