2015-09-21 7:02 AM
Hi,
I'm trying to send data via USART2 but I can't receive anything. Here is my source code: /* Includes ------------------------------------------------------------------*/ &sharpinclude ''stm32l0xx_hal.h'' /* USER CODE BEGIN Includes */ /* USER CODE END Includes */ /* Private variables ---------------------------------------------------------*/ USART_HandleTypeDef husart2; /* USER CODE BEGIN PV */ /* Private variables ---------------------------------------------------------*/ /* USER CODE END PV */ /* Private function prototypes -----------------------------------------------*/ void SystemClock_Config(void); static void MX_GPIO_Init(void); static void MX_USART2_Init(void); void sendOk(void); void sendError(void); /* USER CODE BEGIN PFP */ /* Private function prototypes -----------------------------------------------*/ /* USER CODE END PFP */ /* USER CODE BEGIN 0 */ /* USER CODE END 0 */ int main(void) { /* USER CODE BEGIN 1 */ /* USER CODE END 1 */ /* MCU Configuration----------------------------------------------------------*/ /* Reset of all peripherals, Initializes the Flash interface and the Systick. */ HAL_Init(); /* Configure the system clock */ SystemClock_Config(); /* Initialize all configured peripherals */ MX_GPIO_Init(); MX_USART2_Init(); /* USER CODE BEGIN 2 */ char data[] = ''ABC''; HAL_GPIO_WritePin(GPIOA,GPIO_PIN_5,GPIO_PIN_SET); HAL_Delay(3000); HAL_GPIO_WritePin(GPIOA,GPIO_PIN_5,GPIO_PIN_RESET); /* Infinite loop */ /* USER CODE BEGIN WHILE */ while (1) { /* USER CODE END WHILE */ if( HAL_USART_Transmit( &husart2, (uint8_t *) data, 3, 5000 ) != HAL_OK ) { sendError(); } else { sendOk(); } HAL_GPIO_WritePin(GPIOA,GPIO_PIN_5,GPIO_PIN_RESET); HAL_Delay(3000); /* USER CODE BEGIN 3 */ } /* USER CODE END 3 */ } void sendOk() { HAL_GPIO_WritePin(GPIOA,GPIO_PIN_5,GPIO_PIN_SET); HAL_Delay(2000); HAL_GPIO_WritePin(GPIOA,GPIO_PIN_5,GPIO_PIN_RESET); } void sendError() { for(int i=0; i<3; i++) { HAL_Delay(500); HAL_GPIO_TogglePin(GPIOA,GPIO_PIN_5); } HAL_GPIO_WritePin(GPIOA,GPIO_PIN_5,GPIO_PIN_RESET); } /** System Clock Configuration */ void SystemClock_Config(void) { RCC_OscInitTypeDef RCC_OscInitStruct; RCC_ClkInitTypeDef RCC_ClkInitStruct; RCC_PeriphCLKInitTypeDef PeriphClkInit; __PWR_CLK_ENABLE(); __HAL_PWR_VOLTAGESCALING_CONFIG(PWR_REGULATOR_VOLTAGE_SCALE1); RCC_OscInitStruct.OscillatorType = RCC_OSCILLATORTYPE_MSI; RCC_OscInitStruct.MSIState = RCC_MSI_ON; RCC_OscInitStruct.MSICalibrationValue = 0; RCC_OscInitStruct.MSIClockRange = RCC_MSIRANGE_5; RCC_OscInitStruct.PLL.PLLState = RCC_PLL_NONE; HAL_RCC_OscConfig(&RCC_OscInitStruct); RCC_ClkInitStruct.ClockType = RCC_CLOCKTYPE_SYSCLK; RCC_ClkInitStruct.SYSCLKSource = RCC_SYSCLKSOURCE_MSI; RCC_ClkInitStruct.AHBCLKDivider = RCC_SYSCLK_DIV1; RCC_ClkInitStruct.APB1CLKDivider = RCC_HCLK_DIV1; RCC_ClkInitStruct.APB2CLKDivider = RCC_HCLK_DIV1; HAL_RCC_ClockConfig(&RCC_ClkInitStruct, FLASH_LATENCY_0); PeriphClkInit.PeriphClockSelection = RCC_PERIPHCLK_USART2; PeriphClkInit.Usart2ClockSelection = RCC_USART2CLKSOURCE_PCLK1; HAL_RCCEx_PeriphCLKConfig(&PeriphClkInit); HAL_SYSTICK_Config(HAL_RCC_GetHCLKFreq()/1000); HAL_SYSTICK_CLKSourceConfig(SYSTICK_CLKSOURCE_HCLK); } /* USART2 init function */ void MX_USART2_Init(void) { GPIO_InitTypeDef GPIO_InitStruct; GPIO_InitStruct.Pin = GPIO_PIN_2; GPIO_InitStruct.Mode = GPIO_MODE_AF_PP; GPIO_InitStruct.Pull = GPIO_PULLUP; GPIO_InitStruct.Speed = GPIO_SPEED_FAST; //GPIO_InitStruct.Alternate = GPIO_AF7_USART2; HAL_GPIO_Init(GPIOA, &GPIO_InitStruct); GPIO_InitStruct.Pin = GPIO_PIN_3; GPIO_InitStruct.Mode = GPIO_MODE_AF_PP; GPIO_InitStruct.Pull = GPIO_PULLUP; GPIO_InitStruct.Speed = GPIO_SPEED_FAST; //GPIO_InitStruct.Alternate = GPIO_AF7_USART2; HAL_GPIO_Init(GPIOA, &GPIO_InitStruct); husart2.Instance = USART2; husart2.Init.BaudRate = 9600; husart2.Init.WordLength = USART_WORDLENGTH_8B; husart2.Init.StopBits = USART_STOPBITS_1; husart2.Init.Parity = USART_PARITY_NONE; husart2.Init.Mode = USART_MODE_TX_RX; husart2.Init.CLKPolarity = USART_POLARITY_LOW; husart2.Init.CLKPhase = USART_PHASE_1EDGE; husart2.Init.CLKLastBit = USART_LASTBIT_DISABLE; HAL_USART_Init(&husart2); } /** Pinout Configuration */ void MX_GPIO_Init(void) { /* GPIO Ports Clock Enable */ __GPIOA_CLK_ENABLE(); GPIO_InitTypeDef GPIO_InitStructure; GPIO_InitStructure.Pin = GPIO_PIN_5; GPIO_InitStructure.Speed = GPIO_SPEED_FAST; GPIO_InitStructure.Pull = GPIO_PULLUP; GPIO_InitStructure.Mode = GPIO_MODE_OUTPUT_PP; HAL_GPIO_Init(GPIOA,&GPIO_InitStructure); } /* USER CODE BEGIN 4 */ /* USER CODE END 4 */ &sharpifdef USE_FULL_ASSERT /** * @brief Reports the name of the source file and the source line number * where the assert_param error has occurred. * @param file: pointer to the source file name * @param line: assert_param error line source number * @retval None */ void assert_failed(uint8_t* file, uint32_t line) { /* USER CODE BEGIN 6 */ /* User can add his own implementation to report the file name and line number, ex: printf(''Wrong parameters value: file %s on line %d\r\n'', file, line) */ /* USER CODE END 6 */ } &sharpendif /** * @} */ /** * @} */ I checked twice the terminal baud rate, parity bits, port. Every thin is configured Ok but I don't receive any data. #stm32l0-usart-cube-nucle2015-09-22 3:33 AM
Hi,
I'd highly recommend you to start from UART examples under STM32Cube L0 package: STM32Cube_FW_L0_V1.1.0\Projects\STM32L053R8-Nucleo\Examples\UART, it can be very useful.-Syrine –2015-09-23 3:42 AM
I started with examples but I can't understand how to configure USART1 to send data over the on board USB connector.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.