2018-05-15 2:32 PM
Is there a good example or apnote on the proper use of sleep on exit from an IRQ?
Do I need the Data Synchronization Barrier instruction? (to ensure sleep)
here is some pseudo code, this does appear to work fine. I can see the main loop run once on exit without the '
LL_LPM_EnableSleepOnExit()' and the intended result (no main loop cycle) with it enabled.
I'm not using the HAL in this application, just the LL interface.
void EXTI4_IRQHandler(void)
{ /* Manage Flags */ if(LL_EXTI_IsActiveFlag_0_31(LL_EXTI_LINE_4) != RESET) { /* Clear EXTI flag */ LL_EXTI_ClearFlag_0_31(LL_EXTI_LINE_4); Inputpin_Callback(); } LL_LPM_EnableSleepOnExit(); __DSB();}We’re moving the ST Community to a new platform to give you a better and more reliable community experience.