2019-04-28 6:34 AM
Dear Members,
Can I use SIM900 without SIM card for init code ?
Does it support 3G ?
Thanks
2019-04-28 7:20 AM
It won't allow for much of a network connection. You'll likely just get a registration denied status from AT CREG, and only be able to place emergency calls.
All the AT commands will continue to work, and return errors where network connectivity is required.
2019-04-28 4:51 PM
Can't I get IMEI ? or I need SIM card for it ?
Thanks
2019-04-28 8:24 PM
Here's the output :
SIM900 RTOS TEST BEGIN!
SIM 900 INIT SIM80x_INIT!
SIM 900 INIT DONE!
GET IMEI!
Sim80x_GetIMEI() <--- OK
Sim80x_GetLoadVol() <--- ERROR
Sim80x_GetRingVol() <--- ERROR
Sim80x_GetMicGain() <--- ERROR
Sim80x_GetToneVol() <--- ERROR
Is my UART working properly already ?
The code :
static void SIM900_Thread1(void const *argument)
{
Sim80x_Init(osPriorityLow);
Sim80x_InitValue();
}Thanks
2019-04-28 9:01 PM
The IMEI number belongs to the MODEM
>>Is my UART working properly already ?
I'd know this how? Perhaps show the characters you send to the modem, and those it responds back with?
2019-04-29 8:31 PM
This is the response, do you reckon, it's connected properly ?
SIM900 RTOS TEST BEGIN!
SIM 900 INIT SIM80x_INIT!
AT
O
T
T
OO
SIM 900 INIT DONE!
KKEE
00
11
GET IMEI!
K
Sim80x_GetIMEI() <--- OK
11
55
Sim80x_GetLoadVol() <--- ERROR
K
Sim80x_GetRingVol() <--- ERROR
K
Sim80x_GetMicGain() <--- ERROR
,
Sim80x_GetToneVol() <--- ERROR
,K I put baudrate at 19200 and it's SIM900 for arduino uno shield,
Anyone else have an experiences?
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.