2019-11-08 4:40 AM
I faced up with the issue, I have a while(1) loop in main.c where the leds are blinking or just printf some text. SPI in slave mode and is interrupted when new data are available. But when I got all data, my loop in main.c doesn't print anything and not blinking leds. So before SPI's irq everything printing and blinking, after bytes are received there are no blinking and printing
You can find my code below
// SPI.c
#include "SPI.h"
#include "stdio.h"
#include "stm32f10x.h"
void SPI_Init(void) {
GPIO_InitTypeDef GPIO_InitDef;
SPI_InitTypeDef SPI_InitDef;
NVIC_InitTypeDef NVIC_InitStructure;
// initialize init structs
GPIO_StructInit(&GPIO_InitDef);
SPI_StructInit(&SPI_InitDef);
// initialize clocks
RCC_APB2PeriphClockCmd(RCC_APB2Periph_SPI1 | RCC_APB2Periph_AFIO | RCC_APB2Periph_GPIOA, ENABLE);
// initialize A4/SS A5/SCK A7/MOSI alternate function open-drain (50 MHz)
GPIO_InitDef.GPIO_Pin = GPIO_Pin_4 | GPIO_Pin_5 | GPIO_Pin_7;
GPIO_InitDef.GPIO_Mode = GPIO_Mode_AF_OD;
GPIO_InitDef.GPIO_Speed = GPIO_Speed_50MHz;
GPIO_Init(GPIOA, &GPIO_InitDef);
// initialize A6/MISO alternate function push-pull (50 MHz)
GPIO_InitDef.GPIO_Pin = GPIO_Pin_6;
GPIO_InitDef.GPIO_Mode = GPIO_Mode_AF_PP;
GPIO_InitDef.GPIO_Speed = GPIO_Speed_50MHz;
GPIO_Init(GPIOA, &GPIO_InitDef);
// initialize SPI slave
// for slave, no need to define SPI_BaudRatePrescaler
SPI_InitDef.SPI_Direction = SPI_Direction_2Lines_FullDuplex;
SPI_InitDef.SPI_Mode = SPI_Mode_Slave;
SPI_InitDef.SPI_DataSize = SPI_DataSize_8b; // 8-bit transactions
SPI_InitDef.SPI_FirstBit = SPI_FirstBit_MSB; // MSB first
SPI_InitDef.SPI_CPOL = SPI_CPOL_Low; // CPOL = 0, clock idle low
SPI_InitDef.SPI_CPHA = SPI_CPHA_2Edge; // CPHA = 2
SPI_InitDef.SPI_NSS = SPI_NSS_Soft; // use hardware SS
SPI_InitDef.SPI_BaudRatePrescaler = SPI_BaudRatePrescaler_64; // APB2 72/64 = 1.125 MHz
SPI_InitDef.SPI_CRCPolynomial = 7;
SPI_Init(SPI1, &SPI_InitDef);
SPI_Cmd(SPI1, ENABLE);
NVIC_EnableIRQ(SPI1_IRQn);
//Enable SPI's IRQ
SPI_I2S_ITConfig(SPI1, SPI_I2S_IT_RXNE, ENABLE);
printf("SPI bus init success...\r\n");
}
void SPI_RW() {
while(SPI_I2S_GetFlagStatus(SPI1, SPI_I2S_IT_RXNE) == RESET);
return SPI_I2S_ReceiveData(SPI1);
}
// main.c
#include "stm32f10x.h"
#include "stm32f10x_gpio.h"
#include "stm32f10x_rcc.h"
#include "stm32f10x_spi.h"
#include "SPI.h"
#ifdef OS_USE_SEMIHOSTING
extern void initialise_monitor_handles(void);
#endif
static void SysTickConfig(void) {
/* Setup SysTick Timer for 10ms interrupts */
if (SysTick_Config(SystemCoreClock / 1000))
{
/* Capture error */
while (1);
}
/* Configure the SysTick handler priority */
NVIC_SetPriority(SysTick_IRQn, 1); // if I change Priority to 0 then I can't catch SPI' interruption
}
uint8_t RX_LEN = 32;
uint8_t RX_BUF[RX_LEN] = {0};
void print_buf(uint8_t len) {
for (uint8_t i=0; i<len; i++) {
printf("0x%02x \r\n", RX_BUF[i]);
}
printf("\r\n");
}
void SPI1_IRQn(void) {
for (uint8_t i=0; i<RX_LEN; i++) {
RX_BUF[i] = SPI_RW();
}
print_buf(RX_LEN);
}
void main() {
/* Enable semihosting */
#ifdef OS_USE_SEMIHOSTING
initialise_monitor_handles();
#endif
/* SysTickConfig */
SysTickConfig();
SPI_Init();
while(1) {
printf("hello\r\n");
}
}
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.