2009-04-28 2:13 AM
sdio pins
2011-05-17 4:10 AM
Hi,
I am having difficulties finding the answer to a simple question: If on a design I only use SDIO_D[3..0], can the other bus signals (SDIO[7..4])be used for other purposes ? or must they stay not connected. Thanks, Laurent2011-05-17 4:10 AM
Yes, you can use a 4-bit SDIO SDCard interface, and use the SDIO_D4 to SDIO_D7 to other purposes.
I don't have much time to peruse the manual, but I can assure you it works since we use I2S2 with MCK enabled (SDIO_D6) while using SDIO on our design on a STM32F103ZE. -RelaxeWe’re moving the ST Community to a new platform to give you a better and more reliable community experience.