2012-03-19 8:21 AM
When writing to an SD card in SPI mode, you can do a multiple block write without pre-defining the length (i.e. send CMD25, send some data blocks, finish with a stop command). However, to do a multiple block write using the SDIO functions it seems that the DPSM requires a data length to be set before a write action can occur. Is there any way around this? For example, could I set this to the maximum (512) then cancel/disable the action once the data write is finished?
Thanks in advance. #stm32-sdioWe’re moving the ST Community to a new platform to give you a better and more reliable community experience.