2019-03-18 12:51 AM
Hello,
I would like to start a new design based on STM32H7x3.
The STM32H7 Evalboard uses a dual voltage level translator between MCU and SD-Card. But this required some extra pins (DIR_0,DIR_1_3, CLK_FB, DIR_CMD) that I need for anothere peripheral.
Could someone confirm that I can directly connect a SD-Card (or eMMC in 4bit mode) only using DATA[0..3], CMD, CLK instead?
Does anyone know of a Evalbord that connects a SD-Card in this "simpe" way to the MCU?
Thank you.
2019-03-18 1:00 AM
Check schematics of F746-Discovery kit.
https://www.st.com/en/evaluation-tools/32f746gdiscovery.html
You may do it with 6 pins for 4-bit SDIO.
2019-03-18 1:28 AM
I've used SD and eMMC directly using classic wiring on NUCLEO H743ZI
I have an other board, also without transceiver.
2019-03-18 1:36 AM
thank you.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.