2009-01-14 4:25 AM
Save my RTC
2011-05-17 3:59 AM
Quote:
I'M SO STUPIDD !!
You are NOT alone! And anyone working with ARM probably is not... Thanks to you and to relaxe - saves many time/effort. (by the way - a calm ''relaxe'' is much appreciated...) 136 years somewhat exceeds the ''normal'' 30 days/30 feet warranty of some... [ This message was edited by: jj.sprague on 14-01-2009 17:44 ]2011-05-17 3:59 AM
Instead of building a whole calendar, try the code below. Just include time.h
And look at the doc here: http://www.cplusplus.com/reference/clibrary/ctime/ Will probably prevent you from reinventing the wheel... -Relaxe. /******************************************************************************* * Function Name : Time_Regulate * Description : Returns the time entered by user, using Hyperterminal. * Input : None * Output : None * return : Current time RTC counter value *******************************************************************************/ u32 Time_Regulate(void) { struct tm t; time_t t_of_day; printf(''\r\n==============Time Settings=====================================''); printf(''\nYear:''); t.tm_year = USART_Scanf(2038)-1900; printf(''\nMonth:''); t.tm_mon = USART_Scanf(12)-1; //Number of months since January. [0-11] Go figure. printf(''\nDay:''); t.tm_mday = USART_Scanf(31); printf(''\nHour:''); t.tm_hour = USART_Scanf(24); printf(''\nMinutes:''); t.tm_min = USART_Scanf(60); printf(''\nSeconds:''); t.tm_sec = USART_Scanf(60); t.tm_isdst = 0; t_of_day = mktime(&t); printf(''\n''); printf(ctime(&t_of_day)); /* Return the value to store in RTC counter register */ return(t_of_day); } /******************************************************************************* * Function Name : USART_Scanf * Description : Gets numeric values from the hyperterminal. * Input : None * Output : None * Return : None *******************************************************************************/ u32 USART_Scanf(u32 value) { u32 index = 0; u32 tmp[10] = {0x30, 0x30, 0x30, 0x30, 0x30, 0x30, 0x30, 0x30, 0x30, 0x30}; u32 indexlength = 0; u32 valuetmp; //Calculate the length (in char) max of user input valuetmp = value; if(value) { indexlength++; } for(valuetmp = value; valuetmp > 9; ++indexlength) { valuetmp = (valuetmp / 10); } index = 10-indexlength; while (index != 10) { /* Loop until RXNE = 1 */ while (USART_GetFlagStatus(USART1, USART_FLAG_RXNE) == RESET) {} tmp[index++] = (USART_ReceiveData(USART1)); if ((tmp[index - 1] < 0x30) || (tmp[index - 1] > 0x39)) { printf(''\n\rPlease enter valid number between 0 and 9''); index--; } else { USART_SendData(USART1, (u8) tmp[index-1]); while (USART_GetFlagStatus(USART1, USART_FLAG_TC) == RESET) {} } } /* Calculate the Corresponding value */ index = (tmp[9] - 0x30) + ((tmp[8] - 0x30) * 10) + ((tmp[7] - 0x30) * 100) + ((tmp[6] - 0x30) * 1000) + ((tmp[5] - 0x30) * 10000) + ((tmp[4] - 0x30) * 100000) + ((tmp[3] - 0x30) * 1000000) + ((tmp[2] - 0x30) * 10000000) + ((tmp[1] - 0x30) * 100000000) + ((tmp[0] - 0x30) * 1000000000); /* Checks */ if (index > value) { printf(''\n\rPlease enter valid number between 0 and %d'', value); return 0xFFFFFFFF; } return index; } [ This message was edited by: relaxe on 14-01-2009 18:27 ]We’re moving the ST Community to a new platform to give you a better and more reliable community experience.