2009-01-12 9:19 AM
Access external flash part using I2C/SPI Interface
2011-05-17 3:58 AM
I need to connect an external NAND/NOR flash to STM32F101Vx.
The option that I am considering is to use is the FSMC interface. In this way this part of the memory will be accesible using the ''uVision'' IDE and related flash loaders. I have to interface a LCD Module too, which requires the FSMC interface. Given this scneario do you think I can connect the external flash using I2C/SPI interface and still be able to access the flash part. I want this flash part to be addressable directly as part of the program memory space. Thanks in advance for your helpWe’re moving the ST Community to a new platform to give you a better and more reliable community experience.