2021-08-12 5:21 PM
Hello,
I am using RTC Wakeup timer in STM32F469NIH6 processor. Low level access is using HAL code.
I's is configured with
RTC.CR.WCKSEL = 0x3
RTC.WTR.WUT = 1
EXTI.IMR.MR22 is set
EXTI.RSTR.M22 is set.
It generates RTC Wakeup Interrupt ~122.09usec. interval for about .8sec. After that no more interrupt.
RTC.ISR.WUTF is set
EXTI.PR.M22 is not set
What could be the reason for not generating interrupt any more.
Thanks.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.