2013-12-03 1:32 PM
Hello Guys,
I am trying to make the RTC timestamp feature works but I couldn't. I have to detect a tamper event during anytime, even if the MCU is turned off, for this reason I have connected a battery to VBAT pin. So there is no doubt that it is powered during a reset or when it is turned off. Also I have seen that the signal of the oscillator is running when the power supply is turned off. So the RTC is running. But I am having troubles to register an event when the power supply is off, simply the timestamp register doesn't change. There is my code. Please help me.#include ''User_stm32f4xx_RTC.h''
RTC_InitTypeDef RTC_InitStructure;
RTC_TimeTypeDef RTC_TimeStructure;
RTC_DateTypeDef RTC_DateStructure;
RTC_TimeTypeDef RTC_TimeStampStructure;
RTC_DateTypeDef RTC_TimeStampDateStructure;
__IO uint32_t SynchPrediv =0, AsynchPrediv =0;
char
RTC_Buffer[50];
/**
* @brief Configure the RTC peripheral with the Tamper feature at the beginning of its use
* @param None
* @retval None
*/
void
User_RTC_TAMP1_Init(
void
)
{
/*Declaring variables for Interruption configuration*/
NVIC_InitTypeDef NVIC_InitStructure;
EXTI_InitTypeDef EXTI_InitStructure;
/* Enable the PWR clock */
RCC_APB1PeriphClockCmd(RCC_APB1Periph_PWR, ENABLE);
/* Allow access to RTC */
PWR_BackupAccessCmd(ENABLE);
/* Configure one bit for preemption priority */
NVIC_PriorityGroupConfig(NVIC_PriorityGroup_1);
/*Clearing the RTC_IT_TAMP1 Flag*/
RTC_ClearITPendingBit(RTC_IT_TAMP1);
/* Enable The external line21 interrupt */
EXTI_ClearITPendingBit(EXTI_Line21);
EXTI_InitStructure.EXTI_Line = EXTI_Line21;
/*The line 21 is connected to RTC Tamper and Time Stamp events*/
EXTI_InitStructure.EXTI_Mode = EXTI_Mode_Interrupt;
/*Although there is an specific handler for TAMP_STAMP */
EXTI_InitStructure.EXTI_Trigger = EXTI_Trigger_Rising;
EXTI_InitStructure.EXTI_LineCmd = ENABLE;
EXTI_Init(&EXTI_InitStructure);
/* Enable TAMPER IRQChannel */
NVIC_InitStructure.NVIC_IRQChannel = TAMP_STAMP_IRQn;
NVIC_InitStructure.NVIC_IRQChannelPreemptionPriority = 1;
NVIC_InitStructure.NVIC_IRQChannelSubPriority = 0;
NVIC_InitStructure.NVIC_IRQChannelCmd = ENABLE;
NVIC_Init(&NVIC_InitStructure);
if
(RTC_ReadBackupRegister(RTC_BKP_DR0) != ALREADY_CONFIG)
{
/*RTC Configuring for the first time*/
User_RTC_Config();
/* Setting and configuring the time*/
//Time_Config_first_time();
/*TAMPER Configuration for the first time*/
User_TAMPER_Config();
/*Write to the first RTC Backup Data Register the user flag ALREADY_CONFIG*/
RTC_WriteBackupRegister(RTC_BKP_DR0, ALREADY_CONFIG);
}
else
{
/* Check if the Power On Reset flag is set */
if
(RCC_GetFlagStatus(RCC_FLAG_PORRST) != RESET)
{
Usart_Send(
''\r\n Ocurrio un Power On Reset ....\n\r''
,USARTPC);
}
/* Check if the Pin Reset flag is set */
if
(RCC_GetFlagStatus(RCC_FLAG_PINRST) != RESET)
{
Usart_Send(
''\r\n Ocurrio un Reset Externo ....\n\r''
,USARTPC);
}
Usart_Send(
''\n\r No se requiere configurar RTC....\n\r''
,USARTPC);
/* Enable the RTC Clock */
RCC_RTCCLKCmd(ENABLE);
/* Wait for RTC APB registers synchronisation */
RTC_WaitForSynchro();
}
/*Disabling the RTC ALARM*/
RTC_AlarmCmd(RTC_Alarm_A, DISABLE);
}
/**
* @brief Configure the RTC peripheral by selecting the clock source.
* @param None
* @retval None
*/
void
User_RTC_Config(
void
)
{
// /* Enable the PWR clock */
// RCC_APB1PeriphClockCmd(RCC_APB1Periph_PWR, ENABLE);
// /* Allow access to RTC */
// PWR_BackupAccessCmd(ENABLE);
#if defined (RTC_CLOCK_SOURCE_LSI) /* LSI used as RTC source clock*/
/* The RTC Clock may varies due to LSI frequency dispersion. */
/* Enable the LSI OSC */
RCC_LSICmd(ENABLE);
/* Wait till LSI is ready */
while
(RCC_GetFlagStatus(RCC_FLAG_LSIRDY) == RESET)
{
}
/* Select the RTC Clock Source */
RCC_RTCCLKConfig(RCC_RTCCLKSource_LSI);
SynchPrediv = 0xFF;
AsynchPrediv = 0x7F;
#elif defined (RTC_CLOCK_SOURCE_LSE) /* LSE used as RTC source clock */
/* Enable the LSE OSC */
RCC_LSEConfig(RCC_LSE_ON);
/* Wait till LSE is ready */
while
(RCC_GetFlagStatus(RCC_FLAG_LSERDY) == RESET)
{
}
/* Select the RTC Clock Source */
RCC_RTCCLKConfig(RCC_RTCCLKSource_LSE);
SynchPrediv = 0xFF;
AsynchPrediv = 0x7F;
#else
#error Please select the RTC Clock source inside the main.c file
#endif /* RTC_CLOCK_SOURCE_LSI */
/* Enable the RTC Clock */
RCC_RTCCLKCmd(ENABLE);
/* Wait for RTC APB registers synchronisation */
RTC_WaitForSynchro();
}
/**
* @brief Configuration of Tamper
* @param None
* @retval None
*/
void
User_TAMPER_Config(
void
)
{
/* Disable the Tamper 1 detection */
RTC_TamperCmd(RTC_Tamper_1, DISABLE);
/* Clear Tamper 1 pin Event(TAMP1F) pending flag */
RTC_ClearFlag(RTC_FLAG_TAMP1F);
/*Selecting PC13 as a Tamper pin*/
RTC_TamperPinSelection(RTC_TamperPin_PC13);
/* Precharge time*/
RTC_TamperPinsPrechargeDuration(RTC_TamperPrechargeDuration_4RTCCLK);
/* Configure the Tamper 1 Trigger */
RTC_TamperTriggerConfig(RTC_Tamper_1, RTC_TamperTrigger_RisingEdge);
/* Enable the Tamper interrupt */
RTC_ITConfig(RTC_IT_TAMP, ENABLE);
/* Clear Tamper 1 pin interrupt pending bit */
RTC_ClearITPendingBit(RTC_IT_TAMP1);
/* Enable The TimeStamp */
RTC_TimeStampOnTamperDetectionCmd(ENABLE);
/* Enable The TimeStamp */
//RTC_TimeStampCmd(RTC_TimeStampEdge_Rising, ENABLE);
/* Enable the Tamper 1 detection */
RTC_TamperCmd(RTC_Tamper_1, ENABLE);
}
// /**
// * @brief Time Configuration
// * @param None
// * @retval None
// */
// void Time_Config_first_time(void)
// {
// /* Set the Time */
// RTC_TimeStructure.RTC_Hours = 9;
// RTC_TimeStructure.RTC_Minutes = 30;
// RTC_TimeStructure.RTC_Seconds = 0;
// /* Set the Date */
// RTC_DateStructure.RTC_Month = RTC_Month_September;
// RTC_DateStructure.RTC_Date = 22;
// RTC_DateStructure.RTC_Year = 13;
// RTC_DateStructure.RTC_WeekDay = RTC_Weekday_Friday;
// /* Calendar Configuration */
// RTC_InitStructure.RTC_AsynchPrediv = AsynchPrediv;
// RTC_InitStructure.RTC_SynchPrediv = SynchPrediv;
// RTC_InitStructure.RTC_HourFormat = RTC_HourFormat_12;
// RTC_Init(&RTC_InitStructure);
//
// /* Check on RTC init */
// if (RTC_Init(&RTC_InitStructure) == ERROR){Usart_Send(''\n\r/!\\***** Falla al inicializar el RTC ********/!\\ \n\r'',USARTPC);}
//
// /* Set Current Time and Date */
// if (RTC_SetTime(RTC_Format_BCD, &RTC_TimeStructure) == ERROR){Usart_Send(''\n\r/!\\***** Falla al setear el tiempo del RTC ********/!\\ \n\r'',USARTPC);}
// if (RTC_SetDate(RTC_Format_BCD, &RTC_DateStructure) == ERROR){Usart_Send(''\n\r/!\\***** Falla al setear la fecha del RTC ********/!\\ \n\r'',USARTPC);}
// }
/**
* @brief Display the current time on the Hyperterminal.
* @param None
* @retval None
*/
void
RTC_TimeShow(
void
)
{
/* Get the current Time */
RTC_GetTime(RTC_Format_BIN, &RTC_TimeStructure);
sprintf(RTC_Buffer,
''\n\r El tiempo actual es : %0.2d:%0.2d:%0.2d \n\r''
, RTC_TimeStructure.RTC_Hours, RTC_TimeStructure.RTC_Minutes, RTC_TimeStructure.RTC_Seconds);
Usart_Send(RTC_Buffer,USARTPC);
}
/**
* @brief Display the current date on the Hyperterminal.
* @param None
* @retval None
*/
void
RTC_DateShow()
{
/* Get the current Time */
RTC_GetDate(RTC_Format_BIN, &RTC_DateStructure);
sprintf(RTC_Buffer,
''\n\r La Fecha es : %0.2d-%0.2d-%0.2d \n\r''
, RTC_DateStructure.RTC_Date, RTC_DateStructure.RTC_Month, RTC_DateStructure.RTC_Year);
Usart_Send(RTC_Buffer,USARTPC);
}
/**
* @brief Display the current TimeStamp (time and date) on the Hyperterminal.
* @param None
* @retval None
*/
void
RTC_TimeStampShow(
void
)
{
/* Get the current TimeStamp */
RTC_GetTimeStamp(RTC_Format_BIN, &RTC_TimeStampStructure, &RTC_TimeStampDateStructure);
sprintf(RTC_Buffer,
''\n\r==============TimeStamp Display (Time and Date)=================\n\r''
);
Usart_Send(RTC_Buffer,USARTPC);
sprintf(RTC_Buffer,
''\n\r The current time stamp time (Hour-Minute-Second) is : %0.2d:%0.2d:%0.2d \n\r''
, RTC_TimeStampStructure.RTC_Hours, RTC_TimeStampStructure.RTC_Minutes, RTC_TimeStampStructure.RTC_Seconds);
Usart_Send(RTC_Buffer,USARTPC);
sprintf(RTC_Buffer,
''\n\r The current timestamp date (WeekDay-Date-Month) is : %0.2d-%0.2d-%0.2d \n\r''
, RTC_TimeStampDateStructure.RTC_WeekDay, RTC_TimeStampDateStructure.RTC_Date, RTC_TimeStampDateStructure.RTC_Month);
Usart_Send(RTC_Buffer,USARTPC);
}
#timestamp #tampe #rtc #stm32
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.