2018-05-12 9:09 PM
Hello guys. I have a problem with RTC. (STM32CubeMX 4.25.1, STM32F103C8T6, )
On the penultimate version there was 1 error in the RTC code. But now added new mistakes.
hrtc.Init.AsynchPrediv = RTC_AUTO_1_SECOND
It does not work. Now it starts only like this:
HAL_RTCEx_SetSecond_IT (& hrtc);
And besides, RTC works somewhere 30% slower, for 360 seconds, it manages to count only ~255 seconds. Earlier RTC worked without delays. How to fix the RTC delay?
ERROR:
LL_PWR_EnableBkUpAccess();
/* Enable BKP CLK enable for backup registers */ LL_APB1_GRP1_EnableClock(LL_APB1_GRP1_PERIPH_BKP);FIX:
HAL_PWR_EnableBkUpAccess();
/* Enable BKP CLK enable for backup registers */ __HAL_RCC_BKP_CLK_ENABLE();ERROR:
hrtc.Instance = RTC;
if(HAL_RTCEx_BKUPRead(&hrtc, RTC_BKP_DR1) != 0x32F2){ hrtc.Init.AsynchPrediv = RTC_AUTO_1_SECOND; hrtc.Init.OutPut = RTC_OUTPUTSOURCE_NONE;FIX:
if (HAL_RTCEx_BKUPRead(&hrtc, RTC_BKP_DR1) != 0x32F2) {
sTime.Hours = 0; sTime.Minutes = 0;#!stm32-!cubemx-!rtc2018-05-14 4:15 AM
Seems to be a problem in hardware, quartz is running at a very strange frequency :\
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.