2015-09-16 10:41 PM
Hello,
I have implemented RTC on STM32l053-Nucleo using CubeMX and CubeL0 HAL libraries. I set and get the time and date in RTC using HAL functions but the RTC is not running, I am getting the same time and date I have set. The crystal oscillator connected to RTC as showed in CubeMX is LSI. My IDE is Keil MDK-5. I have posted my RTC initialization function and main function below (main.c is attached). /****************************** RTC init function **********************/ void MX_RTC_Init(void) { /**Initialize RTC and set the Time and Date */ hrtc.Instance = RTC; hrtc.Init.HourFormat = RTC_HOURFORMAT_12; hrtc.Init.AsynchPrediv= 127; hrtc.Init.SynchPrediv= 255; hrtc.Init.OutPut = RTC_OUTPUT_DISABLE; hrtc.Init.OutPutRemap = RTC_OUTPUT_REMAP_PC13; hrtc.Init.OutPutPolarity = RTC_OUTPUT_POLARITY_HIGH; hrtc.Init.OutPutType = RTC_OUTPUT_TYPE_OPENDRAIN; HAL_RTC_Init(&hrtc); } **********************MAIN FUNCTION******************** int main(void) { /* MCU Configuration----------------------------------------------------------*/ /* Reset of all peripherals, Initializes the Flash interface and the Systick. */ HAL_Init(); /* Configure the system clock */ SystemClock_Config(); /* Initialize all configured peripherals */ MX_GPIO_Init(); MX_RTC_Init(); MX_USART2_UART_Init(); /***********************RTC*********************/ RTC_TimeTypeDef sTime; RTC_DateTypeDef sDate; RTC_AlarmTypeDef sAlarm; sTime.Hours = 9; sTime.Minutes = 30; sTime.Seconds = 0; sTime.SubSeconds = 0; sTime.TimeFormat = RTC_HOURFORMAT12_AM; sTime.DayLightSaving = RTC_DAYLIGHTSAVING_NONE; sTime.StoreOperation = RTC_STOREOPERATION_RESET; HAL_RTC_SetTime(&hrtc, &sTime, FORMAT_BCD); sDate.WeekDay = RTC_WEEKDAY_MONDAY; sDate.Month = RTC_MONTH_AUGUST; sDate.Date = 24; sDate.Year = 15; HAL_RTC_SetDate(&hrtc, &sDate, FORMAT_BCD); /**Enable the Alarm A */ sAlarm.AlarmTime.Hours = 0; sAlarm.AlarmTime.Minutes = 0; sAlarm.AlarmTime.Seconds = 0; sAlarm.AlarmTime.SubSeconds = 0; sAlarm.AlarmTime.TimeFormat = RTC_HOURFORMAT12_AM; sAlarm.AlarmTime.DayLightSaving = RTC_DAYLIGHTSAVING_NONE; sAlarm.AlarmTime.StoreOperation = RTC_STOREOPERATION_RESET; sAlarm.AlarmMask = RTC_ALARMMASK_NONE; sAlarm.AlarmSubSecondMask = RTC_ALARMSUBSECONDMASK_ALL; sAlarm.AlarmDateWeekDaySel = RTC_ALARMDATEWEEKDAYSEL_DATE; sAlarm.AlarmDateWeekDay = 1; sAlarm.Alarm = RTC_ALARM_A; HAL_RTC_SetAlarm(&hrtc, &sAlarm, FORMAT_BCD); RTC_TimeTypeDef gTime; char str[100]; while (1) { HAL_RTC_GetTime(&hrtc, &gTime, FORMAT_BCD); sprintf(str, ''Time -> %d:%d:%d (sub seconds: %d)\n'',sTime.Hours, sTime.Minutes, sTime.Seconds, sTime.SubSeconds); HAL_UART_Transmit(&huart2, str, 100, 5000); HAL_Delay(1000); } }2015-09-17 2:18 AM
Post the content of relevant RCC and RTC registers.
JWWe’re moving the ST Community to a new platform to give you a better and more reliable community experience.