2018-05-08 10:44 AM
Is there somewhere a better description about this feature, than there is in the f070 reference manual? Maybe an example?
I don't quite seem to understand how it's supposed to work. Or does CubeMX handle it somehow incorrectly?
Could it affect DMA somehow?
I have two USARTs in use, both using similar DMA (mostly shared code). The other one is typical RS232 and the other is RS-485 (really RS232 with DE-signal, the line driver is not yet used). The typical RS232 works fine, but the RS-485 doesn't seem to have receive DMA enabled.
#uart-dma #usart2 #rs485 #stm32f070xbSolved! Go to Solution.
2018-05-09 9:18 AM
No worries. The problem was the board - on Nucleo-F070RB the USART2 is connected to the embedded ST-LINK chip as a serial/USB converter device. Tampering with the solder bridges fixed the problem.
2018-05-09 9:18 AM
No worries. The problem was the board - on Nucleo-F070RB the USART2 is connected to the embedded ST-LINK chip as a serial/USB converter device. Tampering with the solder bridges fixed the problem.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.