2008-11-14 6:58 AM
Rom Table Alignment Problems
2011-05-17 3:52 AM
I am trying to place a constant table in flash. When I execute the code and point to the table using the LDR R0, =Table_Start command, the start address of the table is returned offset by +1, which of course, screws up all my data. (Example, Table_Start is 0x080003F4. After execution of the LDR command, R0 contains 0x080003F5).
I'm sure I've screwed up something in the alignment! Here's how I set up the section. I'm using IAR EWARM 5.2. Code is pure assembler. Table_Start: DCW 0,62,124,185,247,309,371,432,494,555,616,677,738,799 DCW 859,920,980,1040,1100,1159,1218,1277,1336,1394,1452,1510,1567,1624 I've tried various alignment schemes, and even defined a separate .rodata section, but none seem to work (admittedly I'm still kinda fuzzy on the alignment issues, but I'm starting to make a bit of sense out of them!) If anyone has any thoughts or experiences, help would be appreciated! Regards,2011-05-17 3:52 AM
LDR is a pseudo instruction. If you load a program address, it switches the LSB to 1
to indicate the Thumb-State of the processor. If you load a data address the LSB is not changed. A second way is to use ADR, then the LSB is not changed too.2011-05-17 3:52 AM
Tibo,
Thanks so much! That solved the problem. I'm new to ARM processors and was aware of the interworking instructions, but obviously don't completely understand them. Not only have you helped me solve my immediate issue, but you've pointed me in the direction toward studying and understanding the details. Thanks again. Regards, RussWe’re moving the ST Community to a new platform to give you a better and more reliable community experience.