2011-01-19 11:47 PM
RMII or MII?
2011-05-17 5:22 AM
2011-05-17 5:22 AM
Yep, ETH_RMII_REF_CLK is the input for the 50Mhz clock for the STM32 MAC. In normal RMII mode, the same clock has to be applied on PHY REF_CLK input.
When using the ''25MHz Mode'' (or ''REF_CLK out mode'', or whatever you call it) the PHY can generate the 50Mhz clock which has to be connected to STM32 ETH_RMII_REF_CLK, of course. Until now I only used the 50MHz generated by the STM32 PLL3. This was proven to be working and has the advantage that only 1 crystal is needed for the whole system. But whatever you do - timing and especially clock jitter has to be within limits.2011-05-17 5:22 AM
2011-05-17 5:22 AM
Yes, I used MCO output from PLL3. One 25MHz crystal is sufficient to generate 50Mhz for RMII and 72Mhz for CPU. But this is for F107. Cannot tell you much about the F207 - only that I think it should be possible, too...
2011-05-17 5:22 AM
2011-05-17 5:22 AM
The F2 supports clock inputs or xtals between 4 and 26 MHz.
So you could use a 25 MHz TCXO, and use whatever combination of PLL dividers/multipliers to get to 120 MHz or a rate you need. I haven't looked at the F2 settings, but other than the key frequencies you require, the actual CPU and BUS speeds can typically be quite flexible, and can usually be tweaked to achieve your bandwidth/power goals.2011-05-17 5:22 AM
2011-05-17 5:22 AM
Yes, system clock is independent from REF_CLK. So using the PHY ''25 MHz Mode'' should not be a problem. But you are doing many new things (new uC, new PHY, new mode..) so according to my (and Murphys) experience, you will have problems... ;)
Anyway, I would really recommend to stay close to some existing design (are F2x demo boards already available?). If the F2x would be sampling to the not-so-important-customers like me, I would already have it placed on my board and could tell you more...We’re moving the ST Community to a new platform to give you a better and more reliable community experience.