cancel
Showing results for 
Search instead for 
Did you mean: 

RK043FN8H-CT672B for STM32F756BGT6?

Mimikakarlo
Associate II

Do I need to use RK043FN8H-CT672B for STM32F756BGT6?

1 ACCEPTED SOLUTION

Accepted Solutions
mƎALLEm
ST Employee

Hello @Mimikakarlo and welcome to the community,

According to the datasheet yes and you need to drive it with LTDC interface over RGB lines.

For more details please refer to the AN4861 "Introduction to LCD TFT display controller LTDC on STM32 MCUs"

Hope it helps.

 

To give better visibility on the answered topics, please click on "Accept as Solution" on the reply which solved your issue or answered your question.

View solution in original post

8 REPLIES 8
Andrew Neil
Super User

@Mimikakarlo wrote:

 RK043FN8H-CT672B 


Are you talking about this display?

https://community.st.com/t5/stm32-mcus-touchgfx-and-gui/display-rk043fn66hs-ctg-from-rocktech/td-p/303812

 

A complex system that works is invariably found to have evolved from a simple system that worked.
A complex system designed from scratch never works and cannot be patched up to make it work.

yes

You'd own the task of writing the driver for the SC7283, and making the determination. Looks like its probably workable.

https://www.orientdisplay.com/pdf/SC7283.pdf

Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..
mƎALLEm
ST Employee

Hello @Mimikakarlo and welcome to the community,

According to the datasheet yes and you need to drive it with LTDC interface over RGB lines.

For more details please refer to the AN4861 "Introduction to LCD TFT display controller LTDC on STM32 MCUs"

Hope it helps.

 

To give better visibility on the answered topics, please click on "Accept as Solution" on the reply which solved your issue or answered your question.

Thank you for youe answer. I have a problem with the RK043FN66HS-CTG display because i want brightness 1000cm/m^2, can you suggest me another display for STM32F756BGT6 with 4.3in, 480 x 272 pixels and 1000cm/m^2?
Thank you!

This is what is used on STM32H743-Eval board: AM-640480G5TNQW-T00H

 

To give better visibility on the answered topics, please click on "Accept as Solution" on the reply which solved your issue or answered your question.

Thank you for your answer, but thus display AM-640480G5TNQW-T00H, has size 5.7'' and brightness 430cm/m^2

Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.