2020-11-24 10:55 AM
I'm using a STM32F070CBT and putting it to stop mode with low power regulator on and waking it up with GPIO events.
In our project, we're using every single pin from the MCU, most of those are timers and GPIOs, NFC tag reader, etc
After waking it up, we're running some code and some delays, and the program is getting stuck on HAL_Delay callings. This is what we're initing again after waking it up from stop mode:
if(htim->Instance==TIM7)
{
HAL_TIM_PWM_Stop(&htim3,TIM_CHANNEL_1);
__HAL_TIM_SET_COMPARE(&htim16,TIM_CHANNEL_1,0);
__HAL_TIM_SET_COMPARE(&htim17,TIM_CHANNEL_1,0);
HAL_GPIO_WritePin(LED_R_GPIO_Port,LED_R_Pin,1);
HAL_GPIO_WritePin(LED_G_GPIO_Port,LED_G_Pin,1);
HAL_GPIO_WritePin(LED_B_GPIO_Port,LED_B_Pin,1);
HAL_GPIO_WritePin(BLE_RESET_GPIO_Port,BLE_RESET_Pin,1);
HAL_GPIO_WritePin(MO2P_GPIO_Port, MO2P_Pin,1);
HAL_GPIO_WritePin(MO1P_GPIO_Port, MO1P_Pin,1);
st25r95SPIHibernate();
HAL_TIM_Base_Stop_IT(&htim7);
HAL_PWR_EnterSTOPMode(PWR_LOWPOWERREGULATOR_ON,PWR_STOPENTRY_WFE);
SystemClock_Config();
Systick1= SysTick->CTRL;
SysTick->CTRL = 0b011;
HAL_ResumeTick();
Systick2 = SysTick->CTRL;
HAL_GPIO_WritePin(LED_B_GPIO_Port,LED_B_Pin,0);
HAL_Delay(2);
__HAL_TIM_SET_COMPARE(&htim14,TIM_CHANNEL_1,400);
// HAL_NVIC_SetPriority(SysTick_IRQn, 0, 0)
hadc.State = HAL_ADC_STATE_RESET;
huart3.gState = HAL_UART_STATE_RESET;
hspi1.State = HAL_SPI_STATE_RESET;
hspi2.State = HAL_SPI_STATE_RESET;
htim14.State = HAL_TIM_STATE_RESET;
MX_USART3_UART_Init();
MX_DMA_Init();
MX_ADC_Init();
MX_SPI1_Init();
MX_SPI2_Init();
HAL_TIM_PWM_Start(&htim3,TIM_CHANNEL_1);
reinit=1;
}This function above is the first place the code returns after waking it up, so we've tried to reinit everything. These are some examples of what we've tried:
Are we forgetting something or calling some functions on the wrong order, or is there another thing we're missing?
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.