2021-07-28 11:45 AM
Hello everyone,
I designed my own board which partly failed.
I used 32768 Hz ceramic crystal for LSE and 8MHz ceramic resonator for HSE.
I can upload my code successfully, but, it doesn't execute unless I disable both LSE and HSE.
I'm not professional designer, but, I carefully followed the design recommendations in AN2867.
My resonator is exactly as st recommends 8MHz with 33pF C_load. please check the pics below.
Y41 MC-146 32.7680KA-A3
Y42 AWSCR-8.00CELA-C33-T3
I have a Murat 16MHz resonator which lying around, so I gave a try, but with no luck.
Can someone help me? Any suggestions are really appreciated !
Regards,
Tommy
Solved! Go to Solution.
2021-07-28 12:02 PM
R41 is way too high. I imagine shorting it would get things to work, but I didn't do the math to determine if it's okay.
2021-07-28 12:02 PM
R41 is way too high. I imagine shorting it would get things to work, but I didn't do the math to determine if it's okay.
2021-07-28 12:17 PM
Thank you for taking your time reading my question!
Maybe you're right because all the documentation which I read says nothing about the R ext resistor (which in my case is R41).
The only thing which mentions it is the HSE current.
With some calculation I found it should be something around 3.3K? Am I right?
2021-07-28 12:48 PM
SOLVED!
Great thanks to TDK and his advice. Replacing Y41 with 3.3 K solved the problem.
It's sure any another value around 3.3 K should work also as long as the HSE current is around 1mA.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.