2018-01-22 6:04 AM
Dear,
I work on CAN bus with STM32F107 MCU.
I arrived to configured CAN 1 with the help of 'CAN Networking' example to send and receive CAN frame but when I try to use the CAN 2 (Slave CAN)? I only can send CAN frame. I can't receive CAN frame.
So my CAN is correctly configured because I can send CAN frame. I think the problem is with the filters (I don't completely understand how it work).
// CAN 2 configuration
can2HwHandle.Init.Prescaler = 18;
can2HwHandle.Init.Mode = CAN_MODE_NORMAL; can2HwHandle.Init.SJW = CAN_SJW_1TQ; can2HwHandle.Init.BS1 = CAN_BS1_8TQ; can2HwHandle.Init.BS2 = CAN_BS2_7TQ; can2HwHandle.Init.TTCM = DISABLE; can2HwHandle.Init.ABOM = DISABLE; can2HwHandle.Init.AWUM = DISABLE; can2HwHandle.Init.NART = DISABLE; can2HwHandle.Init.RFLM = DISABLE; can2HwHandle.Init.TXFP = DISABLE;// CAN 2 clock enable
__HAL_RCC_CAN2_CLK_ENABLE();
if ( HAL_CAN_Init(&can2HwHandle) == HAL_OK ) {
filterConfig.FilterNumber = 0; filterConfig.FilterMode = CAN_FILTERMODE_IDMASK; filterConfig.FilterScale = CAN_FILTERSCALE_32BIT; filterConfig.FilterIdHigh = 0; filterConfig.FilterIdLow = 0; filterConfig.FilterMaskIdHigh = 0; filterConfig.FilterMaskIdLow = 0; filterConfig.FilterFIFOAssignment = CAN_FILTER_FIFO0; filterConfig.FilterActivation = ENABLE; filterConfig.BankNumber = 14; if ( HAL_CAN_ConfigFilter(&can2HwHandle, &filterConfig) == HAL_OK) { if ( HAL_CAN_Receive_IT(&can2HwHandle,CAN_FIFO0) == HAL_OK ) { // CAN 2 ITs configuration. HAL_NVIC_SetPriority(CAN2_TX_IRQn,0,15); HAL_NVIC_EnableIRQ(CAN2_TX_IRQn); HAL_NVIC_SetPriority(CAN2_RX0_IRQn,0,15); HAL_NVIC_EnableIRQ(CAN2_RX0_IRQn);}
}
}
I use the same configuration as example but it don't work.
Maybe someone can help me ?
Solved! Go to Solution.
2018-01-22 11:27 PM
Dear,
I resolved the problem. Thank your both. The solution with the same number for FilterNumber et BankNumber like suggest Mario Popovic. But to work, I needed to used CAN1 when I configured CAN2 filters.
Regards
2018-01-22 6:14 AM
Hello Yannick,
Could you please try to change CAN filter configuration for the following?:
filterConfig.FilterNumber = 14; //change from 0 to 14
filterConfig.BankNumber = 0; //change from 14 to 0
Regards
Szymon
2018-01-22 6:20 AM
Dear,
I trying with your configuration but I don't receive CAN frame.
Regards
2018-01-22 7:03 AM
I think your problem is with the filter and bank configuration. The filter bank specifies which filter numbers are assigned to CAN2. If it's set to 14, then filters 14-27 are assigned to CAN2. So when initializing the filters for CAN2 you must start with
FilterNumber
= BankNumber and increment from there.
For your CAN2 initialization you need to use both:
filterConfig.FilterNumber = 14;
filterConfig.BankNumber = 14;
2018-01-22 7:33 AM
Hello Yannick,
Thanks for your feedback. Some time ago I was developing a simple application for STM32F2, which was demonstrating usage of CAN1 and CAN2, both transission and reception. I compared your code with mine and main difference which I found was the
FilterNumber and
BankNumber values. I agree with you that most probably your issue is related to wrong filter configuration.
Please find attached my main.c and it.c files (with interrupts handlers). Maybe you can review themand you will manage to find more differences between your code and mine.
Regards
Szymon
________________ Attachments : main.c.zip : https://st--c.eu10.content.force.com/sfc/dist/version/download/?oid=00Db0000000YtG6&ids=0680X000006Hy7H&d=%2Fa%2F0X0000000b49%2F11bD9S4jjDxLf.vHqZu7LNmD5WIv0rYRXW_p_MFNfqg&asPdf=falsestm32f2xx_it.c.zip : https://st--c.eu10.content.force.com/sfc/dist/version/download/?oid=00Db0000000YtG6&ids=0680X000006Hy7C&d=%2Fa%2F0X0000000b48%2F_zc_jb.QbnC6v2H56LWW5zzoxdWTepRFD6VJ60YuNIA&asPdf=false2018-01-22 11:27 PM
Dear,
I resolved the problem. Thank your both. The solution with the same number for FilterNumber et BankNumber like suggest Mario Popovic. But to work, I needed to used CAN1 when I configured CAN2 filters.
Regards
2018-03-29 8:25 AM
Hello, How did you solve ?
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.