2009-04-17 6:23 AM
Reseting the STLM75 Temperature sensor
2011-05-17 4:10 AM
I have my I2C drivers working as I can read and write to I2C devices. I'm working with the STLM75 Temperature sensor on the eval board. However, I noticed that if an I2C transfer gets interrupted, I can no longer talk to that device. The simplest case is:
1. Generate a START 2. Reset the processor 3. Generate a START 4. Write Addr -> Always generates Acknowledge Failure Error 5. Reset the processor 6. Works fine I've tried generating various combinations of START/STOPs on every reset, but I can't seem to reset the temp sensor. (if that is even the problem) My code is basically taken directly from STM eval example. Thanks in advance! Dan2011-05-17 4:10 AM
Hello Dan,
I am also facing the same problem you did, in I2C communication with STLM75 temperature sensor. ''Write Addr -> Always generates Acknowledge Failure Error '' I have been receiving this error and trying to figure out how to overcome it. Have you found any solutions? Any advice on this matter is appreciated. Thank you.We’re moving the ST Community to a new platform to give you a better and more reliable community experience.