2015-07-10 8:36 AM
Hi, I am working in a wired point to point communication system but I have a problem receiving characters.
I have two electronics communicating each other through USART. I want to send a char periodically from the transmitter (TX) to the receiver (RX) but RX does not read the same char sent from TX. TX is the development kit STM32F4 Discovery. I have no problems sending chars through USART1 in this kit. For my tests I just send the same char periodically. RX is my own design where I use the microcontroller STM32F405. I use USART2 to receive the chars from TX. The configuration of the USART is the same in TX (USART1) and RX (USART2). It is as follows: void USART1_Config(){ GPIO_InitTypeDef GPIO_InitStructure; USART_InitTypeDef USART_InitStructure; RCC_APB2PeriphClockCmd(RCC_APB2Periph_USART1, ENABLE); // Configure AF (Alternate Function) of pins PA0, PA1 GPIO_PinAFConfig(GPIOA, GPIO_PinSource9, GPIO_AF_USART1); GPIO_PinAFConfig(GPIOA, GPIO_PinSource10, GPIO_AF_USART1); USART_InitStructure.USART_BaudRate = 2400; USART_InitStructure.USART_WordLength = USART_WordLength_8b; USART_InitStructure.USART_StopBits = USART_StopBits_1; USART_InitStructure.USART_Parity = USART_Parity_No; USART_InitStructure.USART_HardwareFlowControl = USART_HardwareFlowControl_None; USART_InitStructure.USART_Mode = USART_Mode_Rx | USART_Mode_Tx; GPIO_InitStructure.GPIO_OType = GPIO_OType_PP; GPIO_InitStructure.GPIO_PuPd = GPIO_PuPd_UP; GPIO_InitStructure.GPIO_Mode = GPIO_Mode_AF; GPIO_InitStructure.GPIO_Speed = GPIO_Speed_2MHz; // Configure USART Tx GPIO_InitStructure.GPIO_Pin = GPIO_Pin_9; GPIO_Init(GPIOA, &GPIO_InitStructure); // Configure USART Rx GPIO_InitStructure.GPIO_Pin = GPIO_Pin_10; GPIO_Init(GPIOA, &GPIO_InitStructure); USART_Init(USART1, &USART_InitStructure); USART_Cmd(USART1, ENABLE); // Config IT NVIC_InitTypeDef NVIC_InitStructure; // Enable the USARTx Interrupt RX NVIC_InitStructure.NVIC_IRQChannel = USART1_IRQn; NVIC_InitStructure.NVIC_IRQChannelPreemptionPriority = 0; NVIC_InitStructure.NVIC_IRQChannelSubPriority = 0; NVIC_InitStructure.NVIC_IRQChannelCmd = ENABLE; NVIC_Init(&NVIC_InitStructure); // Config RX IT USARTx USART_ITConfig(USART1, USART_IT_RXNE, ENABLE); } As I want to check all the characters received in RX I have my interrupt routine as it is indicated next: void USART2_IRQHandler(void){ if(USART_GetITStatus(USART2, USART_IT_RXNE) != RESET) { /* Read one byte from the receive data register */ char rxchar = USART_ReceiveData(USART2); ... } } The problem is that the variable rxchar does not contain the same character sent from TX. I have checked the signal from RX and TX with an oscilloscope and they are the same (as it was expected since the system is wired point-to-point). At this point I suppose that the problem is related to the USART configuration but both have the same. I am completely getting stuck on this and I don't know what can I do. Can anybody help me with this? Thank you very much in advance for your help. Greetings! mnem2015-07-10 9:33 AM
PA9 is not viable for USART1_TX on the STM32F4-DISCO, C49 represents a huge problem.
Got the grounds connected between the boards? Show enough code to actually be able to demonstrate the problem.2015-07-13 1:12 AM
I'm sorry, I forgot to say that in STM32F4-DISCO I use PB6 as USART1_TX and PA10 as USART1_RX.
Regarding to the grounds, yes, they are connected between the boards. And the code is simply like that, in TX I just configure the USART1 and then in the main loop I send all the characters. int main(void){ int i=0; USART1_Config(); for(i=0; i< 2500; i++); //delay while (1){ USART_SendData(USART1, 68); // char D while (!USART_GetFlagStatus(USART1, USART_FLAG_TXE)); }/* Infinite loop */ } Then, in the main() on RX I configure the USART2 and in the interrupt routine in my previous post, I just read the character so with the debug tool I can check the value of the variable containing the expected character but it never agrees on the one sent from RX. mnem2015-07-13 7:27 AM
Ok, I made some progress but still does not work... I made a test with another USART. I was using that USART to communicate with the PC through a bluetooth module. This USART receives commands from the PC and it was working perfectly. I have changed de code to see if that USART receives correctly the character from TX and I found that it works the same way, the cahracter is wrong. The only change I made was that I have changed the baudrate from 19200 to 2400 so I think that the USART is not working well at 2400 bauds in rx.
Maybe the values used by the libraries I use to generate the baud rate are not good. Can anybody show me a piece of code to program the USART at 2400 bauds changing the registers? I suppose I need to specify the good values for the baud rate. Thank you very much for your help in advanced. mnem2015-07-13 7:45 AM
Are you using HSI or HSE base clocks?
The 2400 should have a pretty wide tolerance for error, would suggest you review bit timing with scope to ensure it's not wildly off. There is code in stm32f4xx_usart.c to set the rate. The method is explained/documented in the reference manual. The basic math is USARTx->BRR = APBxClock / Baud As I recall USART1 and 6 are on APB2 (the fast bus), the rest on APB1 ie USART1->BRR = 84000000 / 2400; You could check the current setting, and print computed baud rate as a float, the compute % error in setting. Other than that you're going to need to look a fundamental problems with you hardware, because the USART should be pretty solid.We’re moving the ST Community to a new platform to give you a better and more reliable community experience.