2009-08-31 4:59 AM
Readout unprotect command
2011-05-17 4:22 AM
Hi all,
Does the Readout unprotect command always erase the entire Flash even if the Readout protection was not set? And is the result, the same as the erase entire flash command? To be short, can we use the Readout unprotect command to erase the entire flash instead of the erase command to simplify the Flash loader program? ThanksWe’re moving the ST Community to a new platform to give you a better and more reliable community experience.