2020-09-17 4:14 AM
I am almost new to STM32 boards and need to read the multiple channels of ADC.Firstly,can someone tell me that am I allowed to read voltage from more than 16 pins(as there are 16 channels of ADC). Moreover, I have the following code to read 2 ADC channels using DMA. I am not getting that when ADC channel 1 is read where it's value is stored and how would I retrieve it to compare it with some predefined value?Same case for ADC channel2.Which function to use to read ADC channel 1 value.This is the code.Please give me some starting point:
#include "stm32f4xx.h"
#include "stm32f4_discovery.h"
uint16_t ADC1ConvertedValue[2] = {0,0};//Stores converted vals
void DMA_config()
{
RCC_AHB1PeriphClockCmd(RCC_AHB1Periph_DMA2 ,ENABLE);
DMA_InitTypeDef DMA_InitStruct;
DMA_InitStruct.DMA_Channel = DMA_Channel_0;
DMA_InitStruct.DMA_PeripheralBaseAddr = (uint32_t) 0x4001204C;//ADC1's data register
DMA_InitStruct.DMA_Memory0BaseAddr = (uint32_t)&ADC1ConvertedValue;
DMA_InitStruct.DMA_DIR = DMA_DIR_PeripheralToMemory;
DMA_InitStruct.DMA_BufferSize = 2;
DMA_InitStruct.DMA_PeripheralInc = DMA_PeripheralInc_Disable;
DMA_InitStruct.DMA_MemoryInc = DMA_MemoryInc_Enable;
DMA_InitStruct.DMA_PeripheralDataSize = DMA_PeripheralDataSize_HalfWord;//Reads 16 bit values
DMA_InitStruct.DMA_MemoryDataSize = DMA_MemoryDataSize_HalfWord;//Stores 16 bit values
DMA_InitStruct.DMA_Mode = DMA_Mode_Circular;
DMA_InitStruct.DMA_Priority = DMA_Priority_High;
DMA_InitStruct.DMA_FIFOMode = DMA_FIFOMode_Enable;
DMA_InitStruct.DMA_FIFOThreshold = DMA_FIFOThreshold_HalfFull;
DMA_InitStruct.DMA_MemoryBurst = DMA_MemoryBurst_Single;
DMA_InitStruct.DMA_PeripheralBurst = DMA_PeripheralBurst_Single;
DMA_Init(DMA2_Stream0, &DMA_InitStruct);
DMA_Cmd(DMA2_Stream0, ENABLE);
}
void ADC_config()
{
/* Configure GPIO pins ******************************************************/
ADC_InitTypeDef ADC_InitStruct;
ADC_CommonInitTypeDef ADC_CommonInitStruct;
GPIO_InitTypeDef GPIO_InitStruct;
RCC_AHB1PeriphClockCmd( RCC_AHB1Periph_GPIOA, ENABLE);
RCC_APB2PeriphClockCmd(RCC_APB2Periph_ADC1, ENABLE);//ADC1 is connected to the APB2 peripheral bus
GPIO_InitStruct.GPIO_Pin = GPIO_Pin_0 | GPIO_Pin_1;// PA0,PA1
GPIO_InitStruct.GPIO_Mode = GPIO_Mode_AN;//The pins are configured in analog mode
GPIO_InitStruct.GPIO_PuPd = GPIO_PuPd_NOPULL ;//We don't need any pull up or pull down
GPIO_Init(GPIOA, &GPIO_InitStruct);//Initialize GPIOA pins with the configuration
/* ADC Common Init **********************************************************/
ADC_CommonInitStruct.ADC_Mode = ADC_Mode_Independent;
ADC_CommonInitStruct.ADC_Prescaler = ADC_Prescaler_Div2;
ADC_CommonInitStruct.ADC_DMAAccessMode = ADC_DMAAccessMode_Disabled;
ADC_CommonInitStruct.ADC_TwoSamplingDelay = ADC_TwoSamplingDelay_5Cycles;
ADC_CommonInit(&ADC_CommonInitStruct);
/* ADC1 Init ****************************************************************/
ADC_InitStruct.ADC_Resolution = ADC_Resolution_12b;//Input voltage is converted into a 12bit int (max 4095)
ADC_InitStruct.ADC_ScanConvMode = ENABLE;//The scan is configured in multiple channels
ADC_InitStruct.ADC_ContinuousConvMode = ENABLE;//Continuous conversion: input signal is sampled more than once
ADC_InitStruct.ADC_ExternalTrigConv = DISABLE;
ADC_InitStruct.ADC_ExternalTrigConvEdge = ADC_ExternalTrigConvEdge_None;
ADC_InitStruct.ADC_DataAlign = ADC_DataAlign_Right;//Data converted will be shifted to right
ADC_InitStruct.ADC_NbrOfConversion = 2;
ADC_Init(ADC1, &ADC_InitStruct);//Initialize ADC with the configuration
/* Select the channels to be read from **************************************/
ADC_RegularChannelConfig(ADC1, ADC_Channel_0, 1, ADC_SampleTime_144Cycles);//PA0
ADC_RegularChannelConfig(ADC1, ADC_Channel_1, 2, ADC_SampleTime_144Cycles);//PA1
/* Enable DMA request after last transfer (Single-ADC mode) */
ADC_DMARequestAfterLastTransferCmd(ADC1, ENABLE);
/* Enable ADC1 DMA */
ADC_DMACmd(ADC1, ENABLE);
/* Enable ADC1 */
ADC_Cmd(ADC1, ENABLE);
}
int main(void)
{
DMA_config();
ADC_config();
while(1)
{
ADC_SoftwareStartConv(ADC1);
}
return 0;
}
2020-09-17 4:28 AM
uint16_t ADC1ConvertedValue[2] = {0,0};//Stores converted vals
JW
2020-09-18 5:19 AM
This code finally works for reading two channels but is giving issue for reading 4 channels(in case of 4 channels it shows data of only 2 channels i-e channel 0 and channel 1 but not showing for channel 3 and channel 4 ).Can someone tell why?
#include "stm32f4xx.h"
#include "stm32f4_discovery.h"
volatile uint16_t ADC1ConvertedValue[4] = {0,0,0,0};//Stores converted vals [2] = {0,0}
void DMA_config()
{
RCC_AHB1PeriphClockCmd(RCC_AHB1Periph_DMA2 ,ENABLE);
DMA_InitTypeDef DMA_InitStruct;
DMA_InitStruct.DMA_Channel = DMA_Channel_0;
DMA_InitStruct.DMA_PeripheralBaseAddr = (uint32_t) 0x4001204C;//ADC1's data register
DMA_InitStruct.DMA_Memory0BaseAddr = (uint32_t)&ADC1ConvertedValue;
DMA_InitStruct.DMA_DIR = DMA_DIR_PeripheralToMemory;
DMA_InitStruct.DMA_BufferSize = 4;//2
DMA_InitStruct.DMA_PeripheralInc = DMA_PeripheralInc_Disable;//Disable originally
DMA_InitStruct.DMA_MemoryInc = DMA_MemoryInc_Enable;
DMA_InitStruct.DMA_PeripheralDataSize = DMA_PeripheralDataSize_HalfWord;//Reads 16 bit values _HalfWord
DMA_InitStruct.DMA_MemoryDataSize = DMA_MemoryDataSize_HalfWord;//Stores 16 bit values _Halfword
DMA_InitStruct.DMA_Mode = DMA_Mode_Circular;
DMA_InitStruct.DMA_Priority = DMA_Priority_High;
DMA_InitStruct.DMA_FIFOMode = DMA_FIFOMode_Enable;
DMA_InitStruct.DMA_FIFOThreshold = DMA_FIFOThreshold_HalfFull;//_HalfFull
DMA_InitStruct.DMA_MemoryBurst = DMA_MemoryBurst_Single;
DMA_InitStruct.DMA_PeripheralBurst = DMA_PeripheralBurst_Single;
DMA_Init(DMA2_Stream0, &DMA_InitStruct);
DMA_Cmd(DMA2_Stream0, ENABLE);
}
void ADC_config()
{
/* Configure GPIO pins ******************************************************/
ADC_InitTypeDef ADC_InitStruct;
ADC_CommonInitTypeDef ADC_CommonInitStruct;
GPIO_InitTypeDef GPIO_InitStruct;
RCC_AHB1PeriphClockCmd( RCC_AHB1Periph_GPIOA, ENABLE);
RCC_APB2PeriphClockCmd(RCC_APB2Periph_ADC1, ENABLE);//ADC1 is connected to the APB2 peripheral bus
GPIO_InitStruct.GPIO_Pin = GPIO_Pin_0 | GPIO_Pin_1 | GPIO_Pin_2 | GPIO_Pin_3;// PA0,PA1,PA2,PA3
GPIO_InitStruct.GPIO_Mode = GPIO_Mode_AN;//The pins are configured in analog mode
GPIO_InitStruct.GPIO_PuPd = GPIO_PuPd_NOPULL ;//We don't need any pull up or pull down
GPIO_Init(GPIOA, &GPIO_InitStruct);//Initialize GPIOA pins with the configuration
/* ADC Common Init **********************************************************/
ADC_CommonInitStruct.ADC_Mode = ADC_Mode_Independent;
ADC_CommonInitStruct.ADC_Prescaler = ADC_Prescaler_Div2;
ADC_CommonInitStruct.ADC_DMAAccessMode = ADC_DMAAccessMode_Disabled;
ADC_CommonInitStruct.ADC_TwoSamplingDelay = ADC_TwoSamplingDelay_5Cycles;
ADC_CommonInit(&ADC_CommonInitStruct);
/* ADC1 Init ****************************************************************/
ADC_InitStruct.ADC_Resolution = ADC_Resolution_12b;//Input voltage is converted into a 12bit int (max 4095)
ADC_InitStruct.ADC_ScanConvMode = ENABLE;//The scan is configured in multiple channels
ADC_InitStruct.ADC_ContinuousConvMode = ENABLE;//Continuous conversion: input signal is sampled more than once
ADC_InitStruct.ADC_ExternalTrigConv = DISABLE;
ADC_InitStruct.ADC_ExternalTrigConvEdge = ADC_ExternalTrigConvEdge_None;
ADC_InitStruct.ADC_DataAlign = ADC_DataAlign_Right;//Data converted will be shifted to right
ADC_InitStruct.ADC_NbrOfConversion = 4;
ADC_Init(ADC1, &ADC_InitStruct);//Initialize ADC with the configuration
/* Select the channels to be read from **************************************/
ADC_RegularChannelConfig(ADC1, ADC_Channel_0, 1, ADC_SampleTime_144Cycles);//PA0
ADC_RegularChannelConfig(ADC1, ADC_Channel_1, 2, ADC_SampleTime_144Cycles);//PA1
ADC_RegularChannelConfig(ADC1, ADC_Channel_2, 3, ADC_SampleTime_144Cycles);//PA2
ADC_RegularChannelConfig(ADC1, ADC_Channel_3, 4, ADC_SampleTime_144Cycles);//PA3
/* Enable DMA request after last transfer (Single-ADC mode) */
ADC_DMARequestAfterLastTransferCmd(ADC1, ENABLE);
/* Enable ADC1 DMA */
ADC_DMACmd(ADC1, ENABLE);
/* Enable ADC1 */
ADC_Cmd(ADC1, ENABLE);
}
int main(void)
{
DMA_config();
ADC_config();
while(1)
{
ADC_SoftwareStartConv(ADC1);
//value=ADC_Read();
}
return 0;
}
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.