2025-01-07 5:19 AM - last edited on 2025-01-07 6:14 AM by mƎALLEm
Hi Team,
We are working on STM32U5A9J-DK for one of our application interfaced with Octal SPI Flash.We needed to acheive RWW operation which is supported by our Flash chip and we have used OSPI1 and OSPI2 in multiplexed mode but we are controlling Chip select in software because of the limitation in STM32U5A9 chip and we were able to see Parallel operation of Write and Read which is RWW but an issue is we are unable to read the Bank stat register from the flash chip which gives information of the Bank number which is being Written while Read is happening. Now our doubt is it because of chip select controlled in software its not able to read volatile register properly?
Any input on this?
Sanath
2025-01-07 6:16 AM - edited 2025-01-07 6:24 AM
Hello @Sanath,
This thread has nothing to do do with CubeIDE as your question is related to the product usage. I moved it from STM32CubeIDE forum to STM32 MCU products.
2025-01-07 6:35 AM
As per my knowledge, it is possible that controlling the Chip Select in software may result in some timing issues, especially when attempting to read the volatile Bank Status register.
CS should be managed through software, as the synchronization between read and write operations could be disrupted. It can also prevent accurate reading of the register.
I have read about this one at somewhere at one of the tech based platform.
2025-01-08 2:12 AM
Hi @adamfinch
Below are the steps for performing an RWW (Read-While-Write) operation and the corresponding observations regarding the Bank Stat Register:
So above steps says that its reading wrong value.
So, all these are being done using Chip select controlled in software.
Regards,
Sanath
2025-01-08 2:15 AM
Got it know now! Thanks again
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.