2025-02-23 11:15 AM - last edited on 2025-02-24 12:10 AM by mƎALLEm
I used the code below but not working , did you find the solution ?
void SetPinTristate(GPIO_TypeDef *GPIOx, uint16_t GPIO_Pin)
{
GPIO_InitTypeDef GPIO_InitStruct = {0};
GPIO_InitStruct.Pin = GPIO_Pin;
GPIO_InitStruct.Mode = GPIO_MODE_INPUT; // Switch to input mode
GPIO_InitStruct.Pull = GPIO_NOPULL; // No pull-up, No pull-down
HAL_GPIO_Init(GPIOx, &GPIO_InitStruct);
}
void SetPinOutput(GPIO_TypeDef *GPIOx, uint16_t GPIO_Pin)
{
GPIO_InitTypeDef GPIO_InitStruct = {0};
GPIO_InitStruct.Pin = GPIO_Pin;
GPIO_InitStruct.Mode = GPIO_MODE_OUTPUT_PP; // Push-Pull Output
GPIO_InitStruct.Pull = GPIO_NOPULL;
GPIO_InitStruct.Speed = GPIO_SPEED_FREQ_LOW;
HAL_GPIO_Init(GPIOx, &GPIO_InitStruct);
}
while (1)
{
SetPinOutput(GPIOA, GPIO_PIN_1);
HAL_GPIO_WritePin(GPIOA, GPIO_PIN_1, GPIO_PIN_SET);
HAL_Delay(1000);
SetPinTristate(GPIOA, GPIO_PIN_1); // Switch to Tri-State (Hi-Z)
HAL_Delay(1000);
}
2025-02-23 11:32 AM
>>did you find the solution ?
ELEVEN years later.. probably not going to get the OP back
Which part are you using?
It might be quick just to flip a couple of bits in the GPIO registers.
Not looking unreasonable, perhaps single step or break-point so you can inspect the values and GPIO registers
2025-02-23 10:25 PM
"I attempted to dynamically switch between input and output on both the STM32F401RC and STM32F030F4P6 microcontrollers. However, only the initial configuration takes effect, and subsequent changes do not work as expected. On the ATmega328, this functionality performed flawlessly, but I prefer to implement it on the STM32F030F4P6 due to its lower cost. Unfortunately, I have not yet found a solution."
Also tried these methods:
HAL_GPIO_DeInit(GPIOx, GPIO_Pin);
#define GPIO_MODE_INPUT 0x0U
#define GPIO_MODE_OUTPUT 0x1U
void SetPinMode(GPIO_TypeDef *GPIOx, uint16_t GPIO_Pin, uint32_t mode)
{
uint32_t position;
uint32_t temp;
// Loop through all the pins
for (position = 0U; position < 16U; position++)
{
// Check if the current pin is set in GPIO_Pin
if ((GPIO_Pin & (1U << position)) != 0U)
{
// Calculate the position for MODER register
temp = GPIOx->MODER;
temp &= ~(0x3U << (position * 2U)); // Clear the current mode
temp |= (mode << (position * 2U)); // Set the new mode
GPIOx->MODER = temp;
}
}
}
2025-02-24 12:08 AM
The code I wrote was right; I made a *** mistake: the programmer was in connect mode, and I had to disconnect it to operate.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.