2018-04-14 6:23 AM
I add earlyprintl support for stm32f767igt,and it seems success.i modified the start_kernel() function as below
extern void printascii(const char *);
asmlinkage __visible void __init start_kernel(void){ char *command_line; char *after_dashes; printascii('iysheng debug!!!!'); }i get the console output
iysheng debug!!!![ 0.000000] Booting Linux on physical CPU 0x0
[ 0.000000] Linux version 4.4.0-uc0-g17edafa-dirty (shengyang@red.redzone) (gcc version 5.4.0 (GCC) ) #64 PREEMPT Sat Apr 14 20:21:44 CST 2018[ 0.000000] CPU: ARMv7-M [411fc270] revision 0 (ARMv7M), cr=00000000[ 0.000000] CPU: unknown data cache, unknown instruction cache[ 0.000000] Machine model: STMicroelectronics STM32429i-EVAL board[ 0.000000] bootconsole [earlycon0] enabled[ 0.000000] debug: i.....But when i debug timer function,i add one line code in file uClinux/linux/drivers/clocksource/timer-stm32.c as
static irqreturn_t stm32_clock_event_handler(int irq, void *dev_id)
{ struct stm32_clock_event_ddata *data = dev_id;writel_relaxed(0, data->base + TIM_SR);
data->evtdev.event_handler(&data->evtdev);
printk('iysheng *******\n'); return IRQ_HANDLED;}then i get nothing from console,i get confuzed,why could this happen,clk and timer will init after these code i add in start_kernl().So why that happed ,why could i get nothing from the console?
2018-04-15 4:10 AM
My better advice for you is to go for a newer kernel first. 4.4.0 is more than two year old, and STM32 port had a lot of improvement since.
IMHO, the easiest way to go is to try buildroot, carefully avoiding binutils >=2.29
2018-04-18 11:53 AM
,
,
thanks for your advice,i use a dsb code here to solve this bug,code in arch/arm/mm/proc-v7m.S.
diff --git a/arch/arm/mm/proc-v7m.S b/arch/arm/mm/proc-v7m.S
,
old mode 100755,
new mode 100644,
index b390d32..67d9209,
--- a/arch/arm/mm/proc-v7m.S,
+++ b/arch/arm/mm/proc-v7m.S,
@@ -81,12 +81,11 @@ ENDPROC(cpu_v7m_do_resume),
* This should be able to cover all ARMv7-M cores.,
*/,
__v7m_setup:,
-,
@ Configure the vector table base address,
ldr r0, =BASEADDR_V7M_SCB,
ldr r12, =vector_table,
str r12, [r0, V7M_SCB_VTOR],
-,
+,
@ enable UsageFault, BusFault and MemManage fault.,
ldr r5, [r0, ♯ V7M_SCB_SHCSR],
orr r5, ♯ (V7M_SCB_SHCSR_USGFAULTENA | V7M_SCB_SHCSR_BUSFAULTENA | V7M_SCB_SHCSR_MEMFAULTENA),
@@ -105,25 +104,22 @@ __v7m_setup:,
mov r6, lr @ save LR,
mov r7, sp @ save SP,
ldr sp, =__v7m_setup_stack_top,
- dsb @ ensure data Synchronization Barrier <,
mailto:iysheng@163.com
>,
,
- cpsie i @ enable interrupt,
+ cpsie i,
svc ♯ 0,
-,
-1: cpsid i @disable interrupt,
-,
+1: cpsid i,
str r5, [r12, ♯ 11 * 4] @ restore the original SVC vector entry,
mov lr, r6 @ restore LR,
mov sp, r7 @ restore SP,
-,
+,
@ Special-purpose control register,
mov r1, ♯ 1,
msr control, r1 @ Thread mode has unpriviledged access,
,
- @ Configure the System Control Register to ensure 8-byte stack alignment,
+ @ Configure the System Control Register to ensure 8-byte stack alignment,
@ Note the STKALIGN bit is either RW or RAO.,
- @ ldr r12, [r0, V7M_SCB_CCR] @ system control register,
- @ orr r12, ♯ V7M_SCB_CCR_STKALIGN @ bit 9 of V7M_SCB_CCR if read only,
- @ str r12, [r0, V7M_SCB_CCR],
+ ldr r12, [r0, V7M_SCB_CCR] @ system control register,
+ orr r12, ♯ V7M_SCB_CCR_STKALIGN,
+ str r12, [r0, V7M_SCB_CCR],
ret lr,
ENDPROC(__v7m_setup),
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.