2008-06-03 11:40 AM
RCC_WaitForHSEStartUp() fails
2011-05-17 3:36 AM
Hello,
I am currently debugging my own Hardware that uses an STM32F103T8 and an 8MHz ceramic resonator for clock generation. I copied the RCC_Configuration routine from one of the Examples (FWLib v2 / Smartcard) and the problem is that sometimes the routine does not correctly initialize the HSE because the RCC_WaitForHSEStartUp(); fails (timeout). The oscilloscope shows a clean and stable 8MHz at the ceramicl so I am a bit helpless. I am using Rowley's CrossWorks with the latest libraries and the latest STM32 FWLib. Any ideas? [ This message was edited by: gommel on 03-06-2008 14:35 ]2011-05-17 3:36 AM
related:
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.