cancel
Showing results for 
Search instead for 
Did you mean: 

RCC_CFGR_HRPE Bit? (SysClk Devider)

flyer31
Senior
Posted on March 28, 2013 at 10:12

Hi,

in the file System_ST32F4xx.c of the ST4Discovery examples, I always find the following 2 lines for the clock configuration (SysClk 168MHz):

    /* HCLK = SYSCLK / 1*/

    RCC->CFGR |= RCC_CFGR_HPRE_DIV1;

      

    /* PCLK2 = HCLK / 2*/

    RCC->CFGR |= RCC_CFGR_PPRE2_DIV2;

    

    /* PCLK1 = HCLK / 4*/

    RCC->CFGR |= RCC_CFGR_PPRE1_DIV4;

I understand the meaning for the last 4 lines - here SysClk must be devided by 2 or 4, resp., as the APB1 and APB2 frequencies are limited to 84MHz and 42MHz.

But concerning the first 2 lines, here the RM 6.3.3(RCC_CFGR) states:

Bits 7:4 HPRE: AHB prescaler

Set and cleared by software to control AHB clock division factor. ...

0xxx: system clock not divided

1000: system clock divided by 2

...

So according to this register description, RCC_CFGR_HRPE could be left on its init value of 0. Why is it programmed to the value ''2'' in the ST4Discovery examples? Anyone has any idea?

This discussion is locked. Please start a new topic to ask your question.
3 REPLIES 3
waclawek.jan
Super User
Posted on March 28, 2013 at 12:25

I'd guess that they are autogenerated or simply product of copy/paste. Take it as a template for your code where you might potentially want to use a different divider.

> Why is it programmed to the value ''2'' in the ST4Discovery examples?

In my copy of stm32f4xx.h:

#define  RCC_CFGR_HPRE_DIV1                  ((uint32_t)0x00000000)        /*!< SYSCLK not divided */

Where do you have ''2'' from?

JW

flyer31
Senior
Posted on March 28, 2013 at 16:30

Thank you for your answer.

The command

RCC->CFGR |= RCC_CFGR_HPRE_DIV1

puts HPRE to ''2'' (as DIV1 is the 2nd bit in this HPRE field).

waclawek.jan
Super User
Posted on March 28, 2013 at 16:52

No. The C compiler doesn't know about what is written in reference manual.

Check how 

RCC_CFGR_HPRE_DIV1

is defined in the library files you are including/linking. Chances are, that it's a macro defined as I described above.

JW

[EDIT] Oh, I now see what's the source of your confusion:

#define  RCC_CFGR_HPRE_1                     ((uint32_t)0x00000020)        /*!< Bit 1 */

versus

#define  RCC_CFGR_HPRE_DIV1                  ((uint32_t)0x00000000)        /*!< SYSCLK not divided */

Oдна буква и кака�? разница... ;)

JW

Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.