2019-12-09 9:27 AM
All the STM32L4 reference manuals. describe LPTIM_CFGR
Bit 20 WAVE: Waveform shape
The WAVE bit controls the output shape
0: Deactivate Set-once mode, PWM / One Pulse waveform (depending on OPMODE bit)
OPMODE bit is mentioned nowhere else .
STM32G4 datasheet has
Bit 20 WAVE: Waveform shape
The WAVE bit controls the output shape
0: Deactivate Set-once mode, PWM or One Pulse waveform depending on how the timer was
started, CNTSTRT for PWM or SNGSTRT for One Pulse waveform.
This description does make more sense. Please correct in L4 reference manuals.
2020-01-07 8:54 AM
Hello Uwe,
Yes indeed, the description you find in STM32G4 reference manual is the correct one. The L4 reference manuals will be updated to add the same description.
-Amel
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.