2023-04-25 9:33 PM
Hi Team,
I am using a the SAI Peripheral from the STM32L5 family to read data from a master device. I am employing the DMA peripheral to read the data from SAI. I have a buffer of 32kb and I am using the STM board as a slave device. I am using the HAL_SAI_RxCpltCallback() to detect the buffer full status. However, I see that the DMA data is getting overwritten by the time it reaches the Rx complete callback function, unless I stop the DMA transfer inside the Rx complete callback (which is not preferred for the use case that I am working on). This is seen only for a certain frequencies of FS signal.
Here are my debug steps:
STEP-1: Start SAI DMA transfer
STEP-2: Wait for control to get into the HAL_SAI_RxCpltCallback()
STEP-3: Read the data from the DMA buffer within the HAL_SAI_RxCpltCallback()- Here's where I see the data is being overwritten when I read it.
DMA Settings: Circular Mode, 32 bit word transfer
SAI Settings: 32 bit data * 4 slots , slave mode.
Are there any suggestions to circumvent this issue? Any leads on this would be of help. Thanks in advance.
Regards,
Janani Sunil.
2023-04-25 10:45 PM
Check if that STM32's DMA supports double buffer mode (DBM bit, usually set in DMA's CR register).
If it does support DBM, then you activate that, and in half-complete callback you change the currently unused (check CR's CT bit) destination address register M0AR / M1AR.
If it does not support DBM, you should choose the buffer size more wisely: 32 kB takes a lot time to work on, even if it is only copying data, so you need a smaller buffer which can be worked on in the time it takes new data to arrive (SAI sampling period).
2023-05-07 2:42 AM
Hi @Community member - Thank you for the suggestion. However, I have a question on DBM.
I have activated DBM by calling the HAL_DMAEx_MultiBufferStart_IT(). I have submitted two local buffers :
uint32_t buffer1[400];
uint32_t buffer2[400];
Upon the processor's entry to HAL_SAI_RxHalfCpltCallback() after filling up half of the buffer, I see that both the buffers (ie buffer1 and buffer2) are filled up completely.
How is the callback supposed to work in this case?- Does the processor access the half transfer complete callback after receiving every 200 slots of data?
Thanks,
Janani Sunil
2023-05-07 3:07 AM
2023-05-07 3:13 AM
Hi @AScha.3 - Thank you for your reply.
The above steps work perfect for the single buffer mode.
In case I want to employ a DBM, without using the HAL_DMAEx_MultiBufferStart_IT(), which other way would I tell the processor that the DMA needs to work in double buffer mode? The HAL_DMAEx_MultiBufferStart_IT() accepts two memory addresses with which I can configure both the buffers.
Thanks,
Janani Sunil
2023-05-07 6:46 AM
DMA in Circular Mode can do " double buffer " anyway.
(is the "usual" way to work with dma for continuous data transfers )
the buffer is used in 2 half blocks, thats why you have to use/process both blocks:
so set the buffer 2x size , what as a data-block size you want.
memory addresses are simply : block start, block 1/2 size , block end.
understand now ?
2023-05-08 2:22 AM
AScha.3 is correct, DBM is not needed in most cases.
The Half- / Complete splitting is probably good enough.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.