2015-04-27 9:57 AM
Hello,
I'm working on multi channel ADC reading with DMA. But I'm not clear how coverted ADC data of each channel transfer to the assigned memory location. I used STcubeMX to set two input channels of ADC1 with DMA request. However, my setting read only one channel. I attaced my code below. Please take a look and help me if anyone knows what is the problem. Thank you in advance. /* I used these three HAL_API func. in main func. to initialize and start adc with DMA */HAL_ADC_MspInit(&hadc1); HAL_ADC_Init(&hadc1); HAL_ADC_Start_DMA(&hadc1, (uint32_t*)&adc1Buf[0],2);
/* ADC1 init function: I enabled scan mode, continuouse mode and DMA request.
Also, I configured each channel's rank and sample time*/
void MX_ADC1_Init(void) {
ADC_ChannelConfTypeDef sConfig;
/**Configure the global features of the ADC (Clock, Resolution, Data Alignment and number of conversion)
*/ hadc1.Instance = ADC1; hadc1.Init.ClockPrescaler = ADC_CLOCKPRESCALER_PCLK_DIV6; hadc1.Init.Resolution = ADC_RESOLUTION12b; hadc1.Init.ScanConvMode = ENABLE; hadc1.Init.ContinuousConvMode = ENABLE; hadc1.Init.DiscontinuousConvMode = DISABLE; hadc1.Init.ExternalTrigConvEdge = ADC_EXTERNALTRIGCONVEDGE_NONE; hadc1.Init.DataAlign = ADC_DATAALIGN_RIGHT; hadc1.Init.NbrOfConversion = 2; hadc1.Init.DMAContinuousRequests = ENABLE; hadc1.Init.EOCSelection = EOC_SINGLE_CONV; HAL_ADC_Init(&hadc1);/**Configure for the selected ADC regular channel its corresponding rank in the sequencer and its sample time.
*/ sConfig.Channel = ADC_CHANNEL_5; sConfig.Rank = 1; sConfig.SamplingTime = ADC_SAMPLETIME_3CYCLES; HAL_ADC_ConfigChannel(&hadc1, &sConfig);/**Configure for the selected ADC regular channel its corresponding rank in the sequencer and its sample time.
*/ sConfig.Channel = ADC_CHANNEL_13; sConfig.Rank = 2; HAL_ADC_ConfigChannel(&hadc1, &sConfig);}
/*Below code is setting GPIO and DMA */
/* Peripheral clock enable */ HAL_ADC_MspInit() { __ADC1_CLK_ENABLE(); /**ADC1 GPIO Configuration PC3 ------> ADC1_IN13 PA5 ------> ADC1_IN5 */ GPIO_InitStruct.Pin = GPIO_PIN_3; GPIO_InitStruct.Mode = GPIO_MODE_ANALOG; GPIO_InitStruct.Pull = GPIO_NOPULL; HAL_GPIO_Init(GPIOC, &GPIO_InitStruct);
GPIO_InitStruct.Pin = GPIO_PIN_5;
GPIO_InitStruct.Mode = GPIO_MODE_ANALOG; GPIO_InitStruct.Pull = GPIO_NOPULL; HAL_GPIO_Init(GPIOA, &GPIO_InitStruct);/* Peripheral DMA init*/
hdma_adc1.Instance = DMA2_Stream0; hdma_adc1.Init.Channel = DMA_CHANNEL_0; hdma_adc1.Init.Direction = DMA_PERIPH_TO_MEMORY; hdma_adc1.Init.PeriphInc = DMA_PINC_DISABLE; hdma_adc1.Init.MemInc = DMA_MINC_ENABLE; hdma_adc1.Init.PeriphDataAlignment = DMA_PDATAALIGN_HALFWORD; hdma_adc1.Init.MemDataAlignment = DMA_MDATAALIGN_HALFWORD; hdma_adc1.Init.Mode = DMA_CIRCULAR; //DMA_NORMAL; hdma_adc1.Init.Priority = DMA_PRIORITY_HIGH; hdma_adc1.Init.FIFOMode = DMA_FIFOMODE_DISABLE; HAL_DMA_Init(&hdma_adc1);__HAL_LINKDMA(hadc,DMA_Handle,hdma_adc1);
} #adc #stm32f42015-04-27 10:39 AM
Hi,
I found my problem. Actually, I couldn't understand how adc data transfered to the assigned memory. I figured out, each adc channel's halfword data goes to upper and lower 16bit of my uint32_t adc data buffer.We’re moving the ST Community to a new platform to give you a better and more reliable community experience.