2024-11-27 6:53 AM
Hi all
I'm working with an stm32f4 and I have a question about current consumption on stop mode, on the pin PC1 I have a external pull up 10k connected to 3.3v, before stop mode what is the best mode to avoid PC1 consume 0.33ua ? Right now I have put all gpio in ANALOG, in this mode PC1 avoid connection and 0.33ua are not present ?
2024-11-27 7:01 AM
Where does 0.33uA come from?
A 10k resistor across a 3.3V supply will take 0.33mA (ie, 330uA) - is that what you meant?
@SBaro.11 wrote:on the pin PC1 I have a external pull up 10k connected to 3.3v
The pullup will only pass any current when the pin is driving low - so don't drive the pin low!
In general, for minimum current, set GPIO pins to Analog.
2024-11-27 7:08 AM - edited 2024-11-27 7:11 AM
Ok so if I put PC1 in Analog mode no current pass through my external resistor when I'm in stop mode ? Bad news for me in stop mode I have 480ua current and I hoped that the problem would come from PC1, so my issue coming from another part.
2024-11-27 7:29 AM
@SBaro.11 wrote:Ok so if I put PC1 in Analog mode no current pass through my external resistor .
There will always be some leakage.
@SBaro.11 wrote:in stop mode I have 480ua current and I hoped that the problem would come from PC1,
You could easily check by disconnecting the resistor...
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.