2018-02-12 4:42 AM
Hi,
I am doing a project using STM32L432KC controller and EPCQ256 (32MegaBytes) -QSPI flash, Here I am able to Erase, Write and Read. but I am able to write only 1-4 MegaBytes and then writing is gets stopped (Here I attached a Screenshot where it is get's stopped).
I tried enabling 4ByteAddressMode using below code still it is giving same problem.... is there any Bug in my below Function,
QSPI_StatusTypeDef QSPI_ENABLE_4BYTE_MODE(void)
{ QSPI_CommandTypeDef sCommand;QSPI_WriteEnable(&hqspi);
sCommand.InstructionMode = QSPI_INSTRUCTION_1_LINE; sCommand.Instruction = ENTER_4_BYTE_ADDR_MODE_CMD; sCommand.AddressMode = QSPI_ADDRESS_NONE; sCommand.AlternateByteMode = QSPI_ALTERNATE_BYTES_NONE; sCommand.DataMode = QSPI_DATA_1_LINE; sCommand.DummyCycles = 0; sCommand.DdrMode = QSPI_DDR_MODE_DISABLE; sCommand.DdrHoldHalfCycle = QSPI_DDR_HHC_ANALOG_DELAY; sCommand.SIOOMode = QSPI_SIOO_INST_EVERY_CMD; sCommand.NbData = 0; if (HAL_QSPI_Command(&hqspi, &sCommand, HAL_QPSI_TIMEOUT_DEFAULT_VALUE) != HAL_OK) { Error_Handler(); }}please suggest me how to write Full-Flash-Memory
#clive-one #stm32 #qspi #qspi-flash #nesrine-mWe’re moving the ST Community to a new platform to give you a better and more reliable community experience.