2019-12-30 11:48 AM
Hi ! Stm32f103 TIM3
Counting: UP
Clock 72Mhz
Prescaler: 36-1
Period: 10-1
Pulse : 5
Result: 200khz 50% duty, ok !
But
Counting: center aligned
Clock 72Mhz
Prescaler: 18-1
Period: 10-1
Pulse : 5
Result: 222khz 50% duty
Why? Schould be 200khz also.
Checked with multimeter, confirmed with scope.
Solved! Go to Solution.
2019-12-30 1:56 PM
In the first case, the counter's prescaled clock frequency is 2MHz i.e. input clock period is 0.5us; in one period counter counts 0-1-2-3-4-5-6-7-8-9 i.e. 10 input clock periods = 5us => frequency 200kHz.
In the second case, the counter's prescaled clock frequency is 4MHz i.e. period is 0.25us; in one period counter counts 0-1-2-3-4-5-6-7-8-9-8-7-6-5-4-3-2-1 that's 18 input clock periods = 4.5us => frequency 222kHz, exactly as you've experienced.
JW
2019-12-30 1:56 PM
In the first case, the counter's prescaled clock frequency is 2MHz i.e. input clock period is 0.5us; in one period counter counts 0-1-2-3-4-5-6-7-8-9 i.e. 10 input clock periods = 5us => frequency 200kHz.
In the second case, the counter's prescaled clock frequency is 4MHz i.e. period is 0.25us; in one period counter counts 0-1-2-3-4-5-6-7-8-9-8-7-6-5-4-3-2-1 that's 18 input clock periods = 4.5us => frequency 222kHz, exactly as you've experienced.
JW
2019-12-30 10:55 PM
Thank You very much !
Can You tell me one more thing? How to set Pulse value? Still = 5 ?
low-high-low pulse?
0-1-2-3-4 low -- 5-6-7-8-9-8-7-6-high -- 5-4-3-2-1-low
And update event - at every - 0
?
2019-12-31 2:15 AM
In RM0008, the timer chapters, in description of TIMx_CCMR1 register, the behaviour of OCxM signal (from which the output of the channel is derived) is described in the description of PWM modes set by the OC1M bits. See also the Center-aligned PWM waveforms figure.
Yes, update event happens when the counter reaches 0 (unless there are other circumstances preventing this, e.g. Repetition counter (TIMx_RCR) nonzero in the Advanced timers, or TIMx_CR1.UDIS bit set).
JW
2019-12-31 2:32 AM
Thank You, I will read thids RM chapters then !
Szczęśliwego Nowego Roku Janie :)
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.