2021-11-01 10:54 AM
HI all,
Does anyone know how to configure the One Pulse mode on this chip using the HAL library?
I tried producing a constantly on-pulse on a timer by setting the CCR value to be greater than the ARR value. And it produced no output
P.S: I accounted for the fact that the processor adds +1 to the value of the ARR and it still didnt work.
Any help would suffice
2021-11-01 10:57 AM
Which TIM? The Advanced timers (TIM1 and TIM8 generally) need PWM Output to be explicitly enabled (MOE?)
2021-11-01 10:59 AM
It is the Advanced timer TIM1.
Here is the configuration code
/**
* @brief TIM1 Initialization Function
* @param None
* @retval None
*/
static void MX_TIM1_Init(void)
{
/* USER CODE BEGIN TIM1_Init 0 */
/* USER CODE END TIM1_Init 0 */
TIM_ClockConfigTypeDef sClockSourceConfig = {0};
//TIM_ClearInputConfigTypeDef sClearInputConfig = {0};
TIM_SlaveConfigTypeDef sSlaveConfig = {0};
TIM_MasterConfigTypeDef sMasterConfig = {0};
TIM_OC_InitTypeDef sConfigOC = {0};
TIM_BreakDeadTimeConfigTypeDef sBreakDeadTimeConfig = {0};
/* USER CODE BEGIN TIM1_Init 1 */
/* USER CODE END TIM1_Init 1 */
htim1.Instance = TIM1;
htim1.Init.Prescaler = HF_TIMX_PSC;
htim1.Init.CounterMode = TIM_COUNTERMODE_UP;
htim1.Init.Period = HF_TIMX_ARR;
htim1.Init.ClockDivision = TIM_CLOCKDIVISION_DIV1;
htim1.Init.RepetitionCounter = 0;
htim1.Init.AutoReloadPreload = TIM_AUTORELOAD_PRELOAD_DISABLE;
if (HAL_TIM_Base_Init(&htim1) != HAL_OK)
{
Error_Handler();
}
sClockSourceConfig.ClockSource = TIM_CLOCKSOURCE_INTERNAL;
if (HAL_TIM_ConfigClockSource(&htim1, &sClockSourceConfig) != HAL_OK)
{
Error_Handler();
}
if (HAL_TIM_PWM_Init(&htim1) != HAL_OK)
{
Error_Handler();
}
// sClearInputConfig.ClearInputState = ENABLE;
// sClearInputConfig.ClearInputSource = TIM_CLEARINPUTSOURCE_ETR;
// sClearInputConfig.ClearInputPolarity = TIM_CLEARINPUTPOLARITY_NONINVERTED;
// sClearInputConfig.ClearInputPrescaler = TIM_CLEARINPUTPRESCALER_DIV1;
// sClearInputConfig.ClearInputFilter = 8;
// if (HAL_TIM_ConfigOCrefClear(&htim1, &sClearInputConfig, TIM_CHANNEL_1) != HAL_OK)
// {
// Error_Handler();
// }
// if (HAL_TIM_ConfigOCrefClear(&htim1, &sClearInputConfig, TIM_CHANNEL_2) != HAL_OK)
// {
// Error_Handler();
// }
// if (HAL_TIM_ConfigOCrefClear(&htim1, &sClearInputConfig, TIM_CHANNEL_3) != HAL_OK)
// {
// Error_Handler();
// }
sSlaveConfig.SlaveMode = TIM_SLAVEMODE_RESET;
sSlaveConfig.InputTrigger = TIM_TS_ITR1;
if (HAL_TIM_SlaveConfigSynchronization(&htim1, &sSlaveConfig) != HAL_OK)
{
Error_Handler();
}
sMasterConfig.MasterOutputTrigger = TIM_TRGO_OC4REF;
sMasterConfig.MasterSlaveMode = TIM_MASTERSLAVEMODE_ENABLE;
if (HAL_TIMEx_MasterConfigSynchronization(&htim1, &sMasterConfig) != HAL_OK)
{
Error_Handler();
}
sConfigOC.OCMode = TIM_OCMODE_PWM1;
sConfigOC.Pulse = 0;
sConfigOC.OCPolarity = TIM_OCPOLARITY_LOW;
sConfigOC.OCNPolarity = TIM_OCNPOLARITY_LOW;
sConfigOC.OCFastMode = TIM_OCFAST_DISABLE;
sConfigOC.OCIdleState = TIM_OCIDLESTATE_RESET;
sConfigOC.OCNIdleState = TIM_OCNIDLESTATE_RESET;
if (HAL_TIM_PWM_ConfigChannel(&htim1, &sConfigOC, TIM_CHANNEL_1) != HAL_OK)
{
Error_Handler();
}
if (HAL_TIM_PWM_ConfigChannel(&htim1, &sConfigOC, TIM_CHANNEL_2) != HAL_OK)
{
Error_Handler();
}
if (HAL_TIM_PWM_ConfigChannel(&htim1, &sConfigOC, TIM_CHANNEL_3) != HAL_OK)
{
Error_Handler();
}
sConfigOC.OCPolarity = TIM_OCPOLARITY_HIGH;
if (HAL_TIM_PWM_ConfigChannel(&htim1, &sConfigOC, TIM_CHANNEL_4) != HAL_OK)
{
Error_Handler();
}
sBreakDeadTimeConfig.OffStateRunMode = TIM_OSSR_DISABLE;
sBreakDeadTimeConfig.OffStateIDLEMode = TIM_OSSI_DISABLE;
sBreakDeadTimeConfig.LockLevel = TIM_LOCKLEVEL_OFF;
sBreakDeadTimeConfig.DeadTime = 0;
sBreakDeadTimeConfig.BreakState = TIM_BREAK_ENABLE;
sBreakDeadTimeConfig.BreakPolarity = TIM_BREAKPOLARITY_LOW;
sBreakDeadTimeConfig.AutomaticOutput = TIM_AUTOMATICOUTPUT_DISABLE;
if (HAL_TIMEx_ConfigBreakDeadTime(&htim1, &sBreakDeadTimeConfig) != HAL_OK)
{
Error_Handler();
}
/* USER CODE BEGIN TIM1_Init 2 */
#if (CURRENT_MODE != 0)
LL_TIM_DisableBRK(htim1.Instance);
#endif
LL_TIM_OC_SetDeadTime(htim1.Instance, DEAD_TIME);
/* USER CODE END TIM1_Init 2 */
HAL_TIM_MspPostInit(&htim1);
}
2021-11-01 12:44 PM
/* Start channel 1 */
if (HAL_TIM_PWM_Start(&TimHandle, TIM_CHANNEL_1) != HAL_OK)
{
/* PWM Generation Error */
Error_Handler();
}
or explicitly
/* Enable the main output */
__HAL_TIM_MOE_ENABLE(htim);
2021-11-02 7:04 AM
I think the problem is more hardware based, my design is a bootstrap circuit, so I think my bootstrap capacitor cannot be turned on for so long.
However, the low-side MOSFETs -- which is not bootstrapped -- gets turned on for long.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.