2019-11-07 4:05 AM
Hi,
Could you please let me know the default state(Pull up /Pull down) of GPIOs in STM32F427VGT6. Especially I need to know the default state of GPIOs PC4, PB10, PA7 inorder to verify the strapping options for an external Ethernet phy interface. Iam interfacing KSZ8041NLI (ETH phy , Microchip technology) with STM32F427VGT6 using MII interface. For proper working of PHY i need to set the strap option properly. Kindly reply me as soon as possible.
2019-11-07 4:16 AM
Have a look at the reference manual, especially for exceptions. For F427, if I remember well, default pin state is input, no pull.
2019-11-07 5:02 AM
Sounds like the design expected external pull up/down option.
Pins float until configured.
2019-11-07 6:23 AM
> Pins float until configured.
Except the JTAG pins.
THe RM0090 GPIO chapter is quite clear in this regard.
JW
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.