2013-05-18 6:10 AM
Hello,
I'm currently working on the STM32F100C8, but i'm having problems when trying to program it.When launching the debugger i get the following error:''Program received signal SIGTRAP, Trace/breakpoint trap.0x08000440 in SetSysClockTo24 () at ..\src\system_stm32f10x.c:680680 }''I've tried commenting out most of my code to see if it's anything code related. I also tried the default application (provided by atollic) and still get the same error. I tried erasing all the flash using the ST-Link utility, and then re-flashing, but that does not work either.It seems this might be hardware related, but i don't see how.Does anyone have any ideas on what might be the cause, and how to correct it?Thanks,Alex #stm32f1 #sigtrapWe’re moving the ST Community to a new platform to give you a better and more reliable community experience.