2019-08-26 6:22 AM
Hi,
i am using a NUCLEO STM32L412 board and i want to use SPI and I2C together.
Every bus works for itself - this is OK.
But when i measure the signals, i get SPI clock signal on SDA and vice versa the SDA Signal on SPI SCK. I initialized with CubeMx.
Here my connections:
PA12 - SPI1 MOSI
PA11 - SPI MISO
PA5 - SPI SCK
PB6 - I2C SCL
PB6 - I2C SCL
Attached a scope image (SPI CLK = channel 2)
2019-08-26 7:58 AM
>>NUCLEO STM32L412
Which ONE, the 64-pin NUCLEO-L412RB or 32-pin NUCLEO-L412KB?
Check what code CubeMX generated, and the Alternate Function associated against each pin vs documentation in the Data Sheet.
2019-08-26 8:05 AM
check the schematics, there maybe some solder bridge options and maybe an "arduino" LED on SCK which may drop the voltage amplitude.
2019-08-26 8:14 AM
It is the 32-pin...
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.