2014-08-02 3:32 PM
Hello!
We are working in a product that comunicate with other equipments over ethernet interface over tcp/ip protocol, all works fine but sometimes something happen and just ethernet peripheral stop, all other peripherals SPI, USART, I/Os continue operating. We use Keil TCPNET library I think that there is a error on the driver, on debug when the ethernet stop I could found that TBUS bit of ETH_DMA_SR register was set, reading the datasheet I doesn't understand how to exit from this error. If someone had this same problem and can help me. Thanks.2014-08-02 7:53 PM
Presumably you need to free up some buffers, and then ETH_DMASR = 4 will clear the state
2014-08-03 4:15 AM
Clive1,
I will try, then inform what happen..... thanks for your attention2014-08-04 7:35 AM
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.