2018-01-14 12:20 PM
Hi,
flashing of mentioned chip with ST LINK V2 works perfect, but in special case it fails with:
20:56:49 : STLink USB communication error
20:56:49 : Error occured during program operation!20:56:49 : Programming error @ 0x08007600!20:56:52 : Programmed memory Checksum: 0x004C4AD820:56:53 : Disconnected from device.Can't find reason.
It happens only at one instance of output .hex file. If I delete some lines of code and rebuild (.text gets smaller), it is fine, but also if I add some lines of code (.text size increases) it is fine also.
I tried with output .bin format, I installed latest ST LINK Utillity, updated firmware, tried CLI tools... nothing helps. Tried STLINK V2 ISOL also, the same result.
WIN7 pro 64bit, GCC (Gnu ARM Eclipse)
This are section sizes:
section size addr
.isr_vector 0x30a 0x8000000.inits 0x28 0x800030c.data 0x874 0x20000000.data_CCMRAM 0x0 0x0.bss 0x1730 0x20000874.text 0x8a4e 0x8000334.noinit 0x0 0x20001fa4._check_stack 0x1000 0x20001fa4.comment 0x6e 0x0.ARM.attributes 0x31 0x0.debug_frame 0x5b4 0x0Total 0xc377If I understand correctly, there is enough of FLASH/RAM available (256K/48K), or am I wrong here?
I'm attaching problematic .hex file, in case somebody can check on the same chip.
Thanks for your sugestions in advance!
2018-01-15 7:54 AM
I made some additional tests:
-the same file flashes well to STM32F103RB chip, no problems here
-in ST LINK Utility, I manage to manually paste/coppy fw data from the address when error ocured; interestingly, that worked out well, and MCU was running happy after that.
At this moment I don't have another PCB with the same MCU, but as soon as I get one I'll try if problem persists.
But it looks as there is something wrong with MCU's flash, it has been flashed hundreds of times untill now and it may be a bit 'worn out'.
Still, I wouldn't expect 'STLink USB communication error' message because of burnt flash cell.
I'll mark this as 'solved', but would be glad if somebody can share information or experience on that issue.
Thanks!
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.