2017-07-20 3:55 AM
Refering to page no 167 in en.DM00124865.pdf which is available as STM32F746NG USER MANUAL.
These are following typo errors are found as follows:
Bit 10 ADC3EN: ADC3 clock enable
This bit is set and cleared by software.0: ADC3 clock disabled1: ADC3 clock disabledBit 9 ADC2EN: ADC2 clock enableThis bit is set and cleared by software.0: ADC2 clock disabled1: ADC2 clock disabledBit 8 ADC1EN: ADC1 clock enableThis bit is set and cleared by software.0: ADC1 clock disabled1: ADC1 clock disabledPlease! correct this also as soon as possible.
2017-07-20 5:51 AM
Hi
GUPTA.NEERAJ
,I confirm these typo errors.
This is already noted internally to be correct in the coming release of RM0
Thanks and Best Regards
Imen
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.