2022-06-05 5:38 AM
Hi community...
I am working with HAL_SPI_Transmit for writing an ATMEL eprom .
I continue to have error of timeout when I transmit the buffer of 5 bytes..
Instead when I transmit just a single byte no problemm
Here there is the code
uint8_t addrLow = addr & 0xFF;
uint8_t addrHigh = (addr >> 8);
uint8_t wrenInstruction = WREN_EEPROM; // Value : 0x06
uint8_t buffer[5] = {WRITE_EEPROM, addrHigh, addrLow}; //Value : 0x01
for(uint8_t i = 0 ; i < size ; i++)
{
buffer[3+i] = txBuffer[i];
}
//Chip select//
HAL_GPIO_WritePin(GPIOA, GPIO_PIN_2, RESET);
if(HAL_SPI_Transmit(spi2Handle, &wrenInstruction, 1, TIMEOUT_EEPROM) != HAL_OK)
{
return EEPROM_ERROR;; // no issues here
}
//Chip select//
HAL_GPIO_WritePin(GPIOA, GPIO_PIN_2, SET);
//Chip select//
HAL_GPIO_WritePin(GPIOA, GPIO_PIN_2, RESET);
if(HAL_SPI_Transmit(spi2Handle, buffer, 5, TIMEOUT_EEPROM) != HAL_OK)
{
return EEPROM_ERROR; //always get this error
}
//Chip select//
HAL_GPIO_WritePin(GPIOA, GPIO_PIN_2, SET);
HAL_Delay(10); //10 ms wait for the EEPROM to complete the write cycle
return EEPROM_OK;
}Any ideas thanks a lot ?
In the details I got stuck here with the timeout message from the HAL_SPI_Transmit
while (hspi->TxXferCount > 0U)
{
/* Wait until TXE flag is set to send data */
if (__HAL_SPI_GET_FLAG(hspi, SPI_FLAG_TXE))
{
hspi->Instance->DR = *((uint16_t *)hspi->pTxBuffPtr);
hspi->pTxBuffPtr += sizeof(uint16_t);
hspi->TxXferCount--;
}
else
{
/* Timeout management */
if ((((HAL_GetTick() - tickstart) >= Timeout) && (Timeout != HAL_MAX_DELAY)) || (Timeout == 0U))
{
errorcode = HAL_TIMEOUT;
goto error;
}
}
}
}and the spi config
static void MX_SPI1_Init(void)
{
/* USER CODE BEGIN SPI1_Init 0 */
/* USER CODE END SPI1_Init 0 */
/* USER CODE BEGIN SPI1_Init 1 */
/* USER CODE END SPI1_Init 1 */
/* SPI1 parameter configuration*/
hspi1.Instance = SPI1;
hspi1.Init.Mode = SPI_MODE_MASTER;
hspi1.Init.Direction = SPI_DIRECTION_2LINES;
hspi1.Init.DataSize = SPI_DATASIZE_16BIT;
hspi1.Init.CLKPolarity = SPI_POLARITY_LOW;
hspi1.Init.CLKPhase = SPI_PHASE_1EDGE;
hspi1.Init.NSS = SPI_NSS_HARD_OUTPUT;
hspi1.Init.BaudRatePrescaler = SPI_BAUDRATEPRESCALER_2;
hspi1.Init.FirstBit = SPI_FIRSTBIT_MSB;
hspi1.Init.TIMode = SPI_TIMODE_DISABLE;
hspi1.Init.CRCCalculation = SPI_CRCCALCULATION_DISABLE;
hspi1.Init.CRCPolynomial = 10;
if (HAL_SPI_Init(&hspi1) != HAL_OK)
{
//Error_Handler();
}
/* USER CODE BEGIN SPI1_Init 2 */
/* USER CODE END SPI1_Init 2 */
}Thanks for your help
2022-06-05 3:01 PM
Look here:
hspi1.Init.DataSize = SPI_DATASIZE_16BIT;
What's the MCU type and clock frequency? There might be a problem with too fast toggling of NSS and few others.
2022-06-05 3:11 PM
Hi gbm..
Thanks for the reply
MCU is STM32F429ZIT
Clock frequency is set in this way ..
void SystemClock_Config(void)
{
RCC_ClkInitTypeDef RCC_ClkInitStruct;
RCC_OscInitTypeDef RCC_OscInitStruct;
// Enable Power Control clock
__PWR_CLK_ENABLE();
// The voltage scaling allows optimizing the power consumption when the
// device is clocked below the maximum system frequency, to update the
// voltage scaling value regarding system frequency refer to product
// datasheet.
__HAL_PWR_VOLTAGESCALING_CONFIG(PWR_REGULATOR_VOLTAGE_SCALE1);
// Enable HSE Oscillator and activate PLL with HSE as source
RCC_OscInitStruct.OscillatorType = RCC_OSCILLATORTYPE_HSE;
RCC_OscInitStruct.HSEState = RCC_HSE_ON;
RCC_OscInitStruct.PLL.PLLState = RCC_PLL_ON;
RCC_OscInitStruct.PLL.PLLSource = RCC_PLLSOURCE_HSE;
// This assumes the HSE_VALUE is a multiple of 1MHz. If this is not
// your case, you have to recompute these PLL constants.
RCC_OscInitStruct.PLL.PLLM = (HSE_VALUE/1000000u);
RCC_OscInitStruct.PLL.PLLN = 336;
RCC_OscInitStruct.PLL.PLLP = RCC_PLLP_DIV2;
RCC_OscInitStruct.PLL.PLLQ = 7;
HAL_RCC_OscConfig(&RCC_OscInitStruct);
// Select PLL as system clock source and configure the HCLK, PCLK1 and PCLK2
// clocks dividers
RCC_ClkInitStruct.ClockType = (RCC_CLOCKTYPE_SYSCLK | RCC_CLOCKTYPE_HCLK
| RCC_CLOCKTYPE_PCLK1 | RCC_CLOCKTYPE_PCLK2);
RCC_ClkInitStruct.SYSCLKSource = RCC_SYSCLKSOURCE_PLLCLK;
RCC_ClkInitStruct.AHBCLKDivider = RCC_SYSCLK_DIV1;
RCC_ClkInitStruct.APB1CLKDivider = RCC_HCLK_DIV4;
RCC_ClkInitStruct.APB2CLKDivider = RCC_HCLK_DIV2;
HAL_RCC_ClockConfig(&RCC_ClkInitStruct, FLASH_LATENCY_5);
}Any ideas?
Thanks a lot
2022-06-06 12:06 AM
I gave two hints above. Use them to correct your code.
2022-06-06 1:45 AM
Hi gbm..
Which are the hints?
I suppose to change hspi1.Init.DataSize = SPI_DATASIZE_16BIT
and to use SPI_DATASIZE_8BIT..
static void MX_SPI1_Init(void)
{
/* USER CODE BEGIN SPI1_Init 0 */
/* USER CODE END SPI1_Init 0 */
/* USER CODE BEGIN SPI1_Init 1 */
/* USER CODE END SPI1_Init 1 */
/* SPI1 parameter configuration*/
hspi1.Instance = SPI1;
hspi1.Init.Mode = SPI_MODE_MASTER;
hspi1.Init.Direction = SPI_DIRECTION_2LINES;
hspi1.Init.DataSize = SPI_DATASIZE_8BIT;
hspi1.Init.CLKPolarity = SPI_POLARITY_LOW;
hspi1.Init.CLKPhase = SPI_PHASE_1EDGE;
hspi1.Init.NSS = SPI_NSS_SOFT;
hspi1.Init.BaudRatePrescaler = SPI_BAUDRATEPRESCALER_8;
hspi1.Init.FirstBit = SPI_FIRSTBIT_MSB;
hspi1.Init.TIMode = SPI_TIMODE_DISABLE;
hspi1.Init.CRCCalculation = SPI_CRCCALCULATION_DISABLE;
hspi1.Init.CRCPolynomial = 10;
if (HAL_SPI_Init(&hspi1) != HAL_OK)
{
//Error_Handler();
}
/* USER CODE BEGIN SPI1_Init 2 */
/* USER CODE END SPI1_Init 2 */
}I have tried with 8 BIT and I have the same issue..
Which was the other hint?
Thanks a lot
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.